Go to the source code of this file.
Data Structures | |
struct | PRU_IPC_Attrs |
struct | PRU_IPC_Params |
struct | PRU_IPC_Object |
struct | PRU_IPC_Config |
This struct is used to store configurables for PRU_IPC. More... | |
Typedefs | |
typedef struct PRU_IPC_Config_s * | PRU_IPC_Handle |
A handle that is returned from a PRU_IPC_open() call. This handle is required for calling other PRU_IPC APIs. More... | |
typedef void(* | PRU_IPC_CallbackFxn) (void *args) |
A Callback function required to register callback on data receive if receive interrupt is enabled. More... | |
Functions | |
void | PRU_IPC_init (void) |
This function initializes the PRU_IPC module. More... | |
void | PRU_IPC_deinit (void) |
This function deinitializes the PRU_IPC module. More... | |
void | PRU_IPC_Params_init (PRU_IPC_Params *params) |
Function to set default values of PRU_IPC_Params in params. More... | |
PRU_IPC_Handle | PRU_IPC_open (uint32_t idx, PRU_IPC_Params *params) |
To initialize and configure PRU_IPC instance. More... | |
void | PRU_IPC_close (PRU_IPC_Handle handle) |
To stop/end PRU_IPC instance. More... | |
uint16_t | PRU_IPC_getBlockId (PRU_IPC_Handle handle) |
Reads the id of last written block by PRU from the PRU-Config memory. More... | |
int32_t | PRU_IPC_getData (PRU_IPC_Handle handle, void *container) |
Reads the data from the configured shared memory. More... | |
int32_t | PRU_IPC_sendData (PRU_IPC_Handle handle, void *container) |
Send/Write data to the configured shared memory (generates interrupt to PRU if it is enabled) More... | |