Go to the source code of this file.
|
enum | port_State {
INITIALIZING = 1,
FAULTY = 2,
DISABLED = 3,
LISTENING = 4,
PRE_MASTER = 5,
MASTER = 6,
PASSIVE = 7,
UNCALIBRATED = 8,
SLAVE = 9
} |
| Port States, from IEEE 1588v2. More...
|
|
enum | netWorkProtType {
UDP_IPV4 = 1,
UDP_IPV6 = 2,
IEEE_802_3 = 3,
DEVICE_NET = 4,
CONTROL_NET = 5,
PROFINET = 6,
UNKNOWN = 0xFFFE
} |
| Network Protocol Type. More...
|
|
enum | deviceConfig { TC = 1,
OC = 2,
BOTH = 3
} |
| Current Device configuration. More...
|
|
enum | delayType { E2E = 1,
P2P = 2
} |
| PTP Delay Mechanism Type. From Table 9 of Standard. More...
|
|
enum | ptpFrameTypes_t { NON_SYNC_DELAY_FRAME = 0,
SYNC_FRAME = 1,
DELAY_REQ_FRAME = 2,
DELAY_RESP_FRAME = 3
} |
| PTP Delay Mechanism Type. From Table 9 of Standard. More...
|
|
enum | timeSource {
ATOMIC_CLOCK = 0x10,
GPS = 0x20,
TERRESTRIAL_RADIO = 0x30,
PTP = 0x40,
NTP = 0x50,
HAND_SET = 0x60,
OTHER = 0x90,
INTERNAL_OSCILLATOR = 0xA0
} |
| 802.1AS-rev Enumeration8 More...
|
|
|
int32_t | TimeSync_getRxTimestamp (TimeSync_ParamsHandle_t timeSyncParamsHandle, ptpFrameTypes_t rxFrameType, uint8_t rxPort, uint32_t *nanoseconds, uint64_t *seconds) |
| Reads and provides timestamp of a received event message. More...
|
|
int32_t | TimeSync_config (TimeSync_ParamsHandle_t timeSyncHandle) |
| Function to configure domain number and/or log message intervals and/or sync0 signal start time, pulse width. More...
|
|
int32_t | TimeSync_getTxTimestamp (TimeSync_ParamsHandle_t timeSyncParamsHandle, ptpFrameTypes_t txFrameType, uint8_t txPort, uint32_t *nanoseconds, uint64_t *seconds) |
| Reads and provides timestamp of a transmitted event message. More...
|
|
int8_t | TimeSync_adjTimeSlowComp (TimeSync_ParamsHandle_t timeSyncParamsHandle, int32_t adjOffset) |
| Adjusts the IEP clock by the drift value over one Sync interval. More...
|
|
int32_t | TimeSync_setClockTime (TimeSync_ParamsHandle_t timeSyncParamsHandle) |
| Configures the driver memory. More...
|
|
void | TimeSync_getCurrentTime (TimeSync_ParamsHandle_t timeSyncParamsHandle, uint32_t *nanoseconds, uint64_t *seconds) |
| Returns the current time on device. More...
|
|
void | TimeSync_updateDomainNumberInPTPFrames (TimeSync_ParamsHandle_t timeSyncHandle) |
| Update PTP domain number in TX Buffers. More...
|
|
void | TimeSync_updateLogMessageIntervalInPTPFrames (TimeSync_ParamsHandle_t timeSyncHandle) |
| Update log message interval in PTP TX buffers. More...
|
|
void | TimeSync_updateDscpValueInDelayRequestFrame (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t dscpValue) |
| Update DSCP value in IP header in PTP Delay Request buffer. More...
|
|
◆ lswap
Value: ((((x) & 0xff000000) >> 24) | \
(((x) & 0x00ff0000) >> 8) | \
(((x) & 0x0000ff00) << 8) | \
(((x) & 0x000000ff) << 24))
◆ htonl_ts
#define htonl_ts |
( |
|
l | ) |
(lswap(l)) |
◆ ntohl_ts
#define ntohl_ts |
( |
|
l | ) |
(lswap(l)) |
◆ htons_ts
#define htons_ts |
( |
|
s | ) |
((u_short)((u_short)(s) >> 8) | (u_short)((u_short)(s) << 8)) |
◆ ntohs_ts
◆ TASK_STACK_SIZE
#define TASK_STACK_SIZE (2048) |
◆ ICSS_TIMESYNC_EVENT_BIT0
#define ICSS_TIMESYNC_EVENT_BIT0 (0x000001) |
◆ ICSS_TIMESYNC_EVENT_BIT1
#define ICSS_TIMESYNC_EVENT_BIT1 (0x000002) |
◆ ICSS_TIMESYNC_EVENT_BIT2
#define ICSS_TIMESYNC_EVENT_BIT2 (0x000004) |
◆ ICSS_TIMESYNC_EVENT_BIT3
#define ICSS_TIMESYNC_EVENT_BIT3 (0x000008) |
◆ ICSS_TIMESYNC_EVENT_BIT4
#define ICSS_TIMESYNC_EVENT_BIT4 (0x000010) |
◆ ICSS_TIMESYNC_EVENT_BIT5
#define ICSS_TIMESYNC_EVENT_BIT5 (0x000020) |
◆ ICSS_TIMESYNC_EVENT_BIT6
#define ICSS_TIMESYNC_EVENT_BIT6 (0x000040) |
◆ ICSS_TIMESYNC_EVENT_BIT7
#define ICSS_TIMESYNC_EVENT_BIT7 (0x000080) |
◆ SYNT_DEPTH
Syntonization depth. No. of timestamps stored to do RCF & NRR calculation
◆ TS_NUM_DOMAINS
Number of domains supported by implementation
◆ TS_STATE_MACHINE_FIRST_ADJUSTMENT_DONE
#define TS_STATE_MACHINE_FIRST_ADJUSTMENT_DONE 1 |
Bit 0. Indicates that driver has copied TS value directly to IEP registers
◆ TS_STATE_MACHINE_LINE_DELAY_COMPUTED
#define TS_STATE_MACHINE_LINE_DELAY_COMPUTED 2 |
Bit 1. Indicates that Peer delay or Line delay (in case of E2E) has been computed
◆ TS_STATE_MACHINE_SYNC_INTERVAL_COMPUTED
#define TS_STATE_MACHINE_SYNC_INTERVAL_COMPUTED 4 |
Bit 2. Sync interval computed
◆ TS_STATE_MACHINE_READY_FOR_SYNC
#define TS_STATE_MACHINE_READY_FOR_SYNC 7 |
Mask for all three bits. Indicates that driver is now ready to do synchronization
◆ TS_STATE_MACHINE_DEVICE_IN_SYNC
#define TS_STATE_MACHINE_DEVICE_IN_SYNC 8 |
Bit 3. Device is in sync with master This is continuously monitored
◆ OFFSET_ALGO_BIN_SIZE
#define OFFSET_ALGO_BIN_SIZE 5 |
Bin size used for stabilization algo See design doc for details
◆ OFFSET_ALGO_CLUSTER_SIZE
#define OFFSET_ALGO_CLUSTER_SIZE 3 |
Number of entries used for clustering See design doc for details
◆ TIMESYNC_OK
◆ ERROR_TX_FRAMETYPE_NOTVALID
#define ERROR_TX_FRAMETYPE_NOTVALID (-1) |
◆ ERROR_TX_PORTNUMBER_NOTVALID
#define ERROR_TX_PORTNUMBER_NOTVALID (-2) |
◆ ERROR_HANDLE_INVALID
#define ERROR_HANDLE_INVALID (-3) |
◆ ERROR_RX_FRAMETYPE_NOTVALID
#define ERROR_RX_FRAMETYPE_NOTVALID (-4) |
◆ ERROR_RX_PORTNUMBER_NOTVALID
#define ERROR_RX_PORTNUMBER_NOTVALID (-5) |
◆ TimeSync_txCallBack_t
typedef void(* TimeSync_txCallBack_t) (uint32_t arg, uint32_t arg2) |
Transmit callback function.
◆ TimeSync_SyncLossCallBack_t
typedef void(* TimeSync_SyncLossCallBack_t) (void) |
Sync loss callback function. Call cross module functions in case of loss of synchronization.
◆ TimeSync_stackResetCallback_t
typedef void(* TimeSync_stackResetCallback_t) (void *arg) |
PTP Stack Reset callback function. Timesync handle (of type TimeSync_ParamsHandle_t) will be passed as arg.
◆ TimeSync_ParamsHandle_t
◆ port_State
Port States, from IEEE 1588v2.
Enumerator |
---|
INITIALIZING | |
FAULTY | |
DISABLED | |
LISTENING | |
PRE_MASTER | |
MASTER | |
PASSIVE | |
UNCALIBRATED | |
SLAVE | |
◆ netWorkProtType
Network Protocol Type.
Enumerator |
---|
UDP_IPV4 | IPv4
|
UDP_IPV6 | IPv6
|
IEEE_802_3 | Ethernet without TCP/IP
|
DEVICE_NET | |
CONTROL_NET | |
PROFINET | |
UNKNOWN | |
◆ deviceConfig
Current Device configuration.
Enumerator |
---|
TC | Only Transparent Clock
|
OC | Only Ordinary Clock
|
BOTH | Both OC and TC
|
◆ delayType
PTP Delay Mechanism Type. From Table 9 of Standard.
Enumerator |
---|
E2E | Used for CIP Sync
|
P2P | Used for IEC 61558
|
◆ ptpFrameTypes_t
PTP Delay Mechanism Type. From Table 9 of Standard.
Enumerator |
---|
NON_SYNC_DELAY_FRAME | Non Sync or Delay Req/Res frame
|
SYNC_FRAME | SYNC Frame
|
DELAY_REQ_FRAME | Delay Request Frame
|
DELAY_RESP_FRAME | Delay Response Frame
|
◆ timeSource
802.1AS-rev Enumeration8
Enumerator |
---|
ATOMIC_CLOCK | |
GPS | |
TERRESTRIAL_RADIO | |
PTP | |
NTP | |
HAND_SET | |
OTHER | |
INTERNAL_OSCILLATOR | |