|
AM64x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
87 typedef struct ptcpTimes
104 uint8_t subdomainUUID[16];
194 uint32_t *outRxDelay, uint32_t *outTxDelay);
205 uint32_t *outRxDelay, uint32_t *outTxDelay);
243 uint32_t syncTimeoutFactor);
254 uint32_t takeoverTimeoutFactor);
uint32_t cableDelay
Definition: iPtcpDrv.h:93
uint16_t Status
Definition: iPtcpDrv.h:113
@ disable
Definition: iPtcpDrv.h:62
struct PN_Config_s * PN_Handle
Alias for Profinet Handle containing base addresses and modules.
Definition: PN_Handle.h:96
uint32_t IEP_count_tL_R
Definition: iPtcpDrv.h:130
uint32_t TorgSec
Definition: iPtcpDrv.h:125
void PN_PTCP_getSyncMasterAddress(PN_Handle pnHandle, uint8_t *addr)
Get the sync Master address (MAC)
void PN_PTCP_configureSyncFwd(PRUICSS_HwAttrs const *pruicssHwAttrs, ptcpPortStatus_t state)
Controls(enable/disable) the sync forwarding; by default it is enabled.
@ TAKEOVER_TIMEOUT
Definition: iPtcpDrv.h:75
uint32_t rxDelayLocal
Definition: iPtcpDrv.h:89
@ SYNC_TIMEOUT
Definition: iPtcpDrv.h:76
Structure containing the port delay values of the local and remote.
Definition: iPtcpDrv.h:88
uint8_t state
Definition: tisci_pm_clock.h:3
void PN_PTCP_getDelayValues(PN_Handle pnHandle, ptcpPortDelayVal_t *portDelays, uint8_t portNum)
Returns the current cable delay related values.
uint32_t rxDelayRemote
Definition: iPtcpDrv.h:91
uint32_t Nanoseconds
Definition: iPtcpDrv.h:116
uint64_t addr
Definition: csl_udmap_tr.h:3
void PN_PTCP_registerDelayUpdateCall(PN_Handle pnHandle, ptcpCallBack_t callBack)
Registers the callback function for getting notifications about new cable delay measurement.
@ IN_SYNC
Definition: iPtcpDrv.h:74
uint32_t SecondsLow
Definition: iPtcpDrv.h:115
uint64_t tick_S
Definition: iPtcpDrv.h:134
syncState_t syncState
Definition: iPtcpDrv.h:102
PRUICSS Hardware Attributes.
Definition: pruicss/g_v0/pruicss.h:334
void PN_PTCP_getRemoteDelayValues(PN_Handle pnHandle, uint8_t portNum, uint32_t *outRxDelay, uint32_t *outTxDelay)
Get the remote port delay values.
void PN_PTCP_setTakeoverTimeoutFactor(PN_Handle pnHandle, uint32_t takeoverTimeoutFactor)
Sets the takeover timeout factor.
void PN_PTCP_setSyncUUID(PN_Handle pnHandle, uint8_t *subdomainUUID)
Sets the sync UUID for the device. Application is also notified about the current sync status....
void PN_PTCP_registerSyncStatusCall(PN_Handle pnHandle, ptcpCallBack_t callBack)
Registers the callback function for getting notifications about change in sync state.
void PN_PTCP_setSyncTimeoutFactor(PN_Handle pnHandle, uint32_t syncTimeoutFactor)
Sets the Sync timeout factor.
uint64_t tick_L
Definition: iPtcpDrv.h:135
Definition: iPtcpDrv.h:124
uint32_t IEP_count_fn
Definition: iPtcpDrv.h:132
uint32_t TDelay
Definition: iPtcpDrv.h:127
Definition: iPtcpDrv.h:112
uint16_t SecondsHigh
Definition: iPtcpDrv.h:114
uint64_t tick_fn
Definition: iPtcpDrv.h:136
void PN_PTCP_getSyncInfo(PN_Handle pnHandle, ptcpSyncInfo_t *syncInfo)
Returns current sync status and other sync related info.
void PN_PTCP_configureDelayResp(PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t portNum, ptcpPortStatus_t state)
uint32_t txDelayRemote
Definition: iPtcpDrv.h:92
uint32_t txDelayLocal
Definition: iPtcpDrv.h:90
@ OUT_OF_SYNC
Definition: iPtcpDrv.h:73
uint32_t IEP_count_tL_F
Definition: iPtcpDrv.h:131
void PN_PTCP_latchInit(PN_Handle pnHandle)
uint32_t TorgNsec
Definition: iPtcpDrv.h:126
Structure containing current sync info.
Definition: iPtcpDrv.h:101
syncState_t
Enum for the various sync states.
Definition: iPtcpDrv.h:72
void PN_PTCP_setPllWindow(PN_Handle pnHandle, uint32_t pllWindowSize)
Sets the PLL window for sync handling.
int32_t PN_PTCP_getAbsoluteTime(PN_Handle pnHandle, PNIO_TimeStamp *p_PNIO_TimeStamp, int32_t LatchEn)
API to return absolute PTCP time.
void PN_PTCP_configureDelayMeasurement(PN_Handle pnHandle, uint8_t portNum, ptcpPortStatus_t state)
Controls(enable/disable) the delay measurement process on a particular port. By default,...
uint32_t IEP_count_tS
Definition: iPtcpDrv.h:129
void PN_PTCP_getLocalDelayValues(PN_Handle pnHandle, uint8_t portNum, uint32_t *outRxDelay, uint32_t *outTxDelay)
Get the local port delay values.
ptcpPortStatus_t
Enum for enable/disable states.
Definition: iPtcpDrv.h:61
void(* ptcpCallBack_t)(uint32_t arg, uint32_t arg2)
Definition: iPtcpDrv.h:151
@ enable
Definition: iPtcpDrv.h:63