|
AM64x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
38 #ifndef RED_HSR_HANDLE_H_
39 #define RED_HSR_HANDLE_H_
48 typedef struct hsrPrp_Config_s
ClockP_Object redPruCheckTimer
Definition: hsrPrp_handle.h:65
struct ICSS_EMAC_Config_s * ICSS_EMAC_Handle
Alias for ICSS EMAC Handle containing base addresses and modules.
Definition: icss_emac.h:368
ClockP_Object redLifeCheckTimer
Definition: hsrPrp_handle.h:67
Node Table Entry.
Definition: hsrPrp_red_common.h:491
RED_INDEX_ARRAY_ENTRY * indexArrayBase
Definition: hsrPrp_handle.h:79
Opaque clock object used with the clock APIs.
Definition: ClockP.h:59
Bin array Entry.
Definition: hsrPrp_red_common.h:479
Opaque task object used with the task APIs.
Definition: TaskP.h:94
SemaphoreP_Object redLifeCheckSemaphore
Definition: hsrPrp_handle.h:75
TaskP_Object hsrPrpNodetableRefreshTask
Definition: hsrPrp_handle.h:73
ICSS_EMAC_Handle icssEmacHandle
Definition: hsrPrp_handle.h:59
uint32_t redPruCheckTimerNodeTableClear
Definition: hsrPrp_handle.h:63
hsrPrp_Config Structure storing the global variables
Definition: hsrPrp_handle.h:49
SemaphoreP_Object nodesTableSemaphore
Definition: hsrPrp_handle.h:77
uint32_t redPruCheckTimerHostTableFlag
Definition: hsrPrp_handle.h:61
struct hsrPrp_Config_s hsrPrpHandle
Definition: hsrPrp_handle.h:86
uint16_t supSeqNr
Definition: hsrPrp_handle.h:53
RED_FRAME * redSupFrame
Definition: hsrPrp_handle.h:69
int * num_of_collision_occured
Definition: hsrPrp_handle.h:57
RED_BIN_ARRAY_ENTRY * binArrayBase
Definition: hsrPrp_handle.h:81
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
int * collision_pkt_dropped
Definition: hsrPrp_handle.h:55
Definition: hsrPrp_red_common.h:140
RED_NODE_TABLE_ENTRY * nodeTableBase
Definition: hsrPrp_handle.h:83
Index array Entry.
Definition: hsrPrp_red_common.h:465
uint16_t redSeqNr
Definition: hsrPrp_handle.h:51
TaskP_Object redSupTask
Definition: hsrPrp_handle.h:71