AM64x MCU+ SDK  08.02.00
FSI

The Fast Serial Interface (FSI) driver provides API to program the FSI module. FSI is a serial communication peripheral capable of reliable and robust high-speed communications. FSI is used to transfer/receive data frame with several available configurations e.g frame size, bandwidth etc, signaling events completion via interrupts or status registers.

Features Supported

  • Supports programmable packet data length of 1-to-16 words where each word consists of 16-bits
  • Supports programmable frame tagging (0000-to-1111) for message filtering
  • Supports programmable data-lines( 1-or-2) for communication
  • Supports Double Data Rate (DDR) communication
  • Supports programmable interrupts via 2 interrupt lines per FSI core

Features NOT Supported

  • DMA mode
  • Multi-Slave configuration
  • clkstop_req/ack functionality. Software must ensure that the FSI IP's on both host and remote device are idle before triggering clkstop_req.

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
  • Selection of instances present in the device
  • Configuring pinmux based on selected instance and pin configuration

Important Usage Guidelines

  • Note: FSI-RX and FSI-TX are completely independent and separate module. For communication, both needs to be configured separately.

Example Usage

Include the below file to access the APIs

#include <drivers/fsi.h>

FSI tx config

int32_t status;
/* TX init and reset */
status = FSI_performTxInitialization(txBaseAddr, FSI_APP_TX_PRESCALER_VAL);
status += FSI_resetTxModule(txBaseAddr, FSI_TX_MASTER_CORE_RESET);
FSI_clearTxModuleReset(txBaseAddr, FSI_TX_MASTER_CORE_RESET);
/* Setting for requested transfer params */
status += FSI_setTxSoftwareFrameSize(txBaseAddr, FSI_APP_FRAME_DATA_WORD_SIZE);
status += FSI_setTxDataWidth(txBaseAddr, FSI_APP_N_LANES);
/* Setting frame config */
status += FSI_setTxUserDefinedData(txBaseAddr, FSI_APP_TX_USER_DATA);
status += FSI_setTxFrameTag(txBaseAddr, FSI_APP_TX_DATA_FRAME_TAG);
status += FSI_setTxFrameType(txBaseAddr, FSI_FRAME_TYPE_NWORD_DATA);

FSI rx config

int32_t status;
/* RX init and reset */
status = FSI_performRxInitialization(rxBaseAddr);
status += FSI_resetRxModule(rxBaseAddr, FSI_RX_MASTER_CORE_RESET);
FSI_clearRxModuleReset(rxBaseAddr, FSI_RX_MASTER_CORE_RESET);
/* Setting for requested transfer params */
status += FSI_setRxSoftwareFrameSize(rxBaseAddr, FSI_APP_FRAME_DATA_WORD_SIZE);
status += FSI_setRxDataWidth(rxBaseAddr, FSI_APP_N_LANES);
status += FSI_setRxBufferPtr(rxBaseAddr, 0U);

FSI configuration to enable interrupt

static void Fsi_appTxCallback(void *args)
{
uint32_t txBaseAddr = (uint32_t) args;
FSI_clearTxEvents(txBaseAddr, FSI_TX_EVT_FRAME_DONE);
SemaphoreP_post(&gFsiTxSemObject);
/*
** Handle tx callback function here
*/
return;
}
static void Fsi_appRxCallback(void *args)
{
uint32_t rxBaseAddr = (uint32_t) args;
FSI_clearRxEvents(rxBaseAddr, FSI_RX_EVT_DATA_FRAME);
SemaphoreP_post(&gFsiRxSemObject);
/*
** Handle rx callback function here
*/
return;
}
static int32_t Fsi_appIntrInit(uint32_t txBaseAddr, uint32_t rxBaseAddr)
{
int32_t status;
uint32_t txIntrNum, rxIntrNum;
HwiP_Params txHwiPrms, rxHwiPrms;
/*
* TX interrupt config and registration
*/
txIntrNum = CONFIG_FSI_TX0_INTR1;
status = SemaphoreP_constructBinary(&gFsiTxSemObject, 0);
HwiP_Params_init(&txHwiPrms);
txHwiPrms.intNum = txIntrNum;
txHwiPrms.callback = Fsi_appTxCallback;
txHwiPrms.args = (void *) txBaseAddr;
HwiP_construct(&gFsiTxHwiObject, &txHwiPrms);
/* Enable TX frame done interrupt */
status += FSI_enableTxInterrupt(txBaseAddr, FSI_INT1, FSI_TX_EVT_FRAME_DONE);
/*
* RX interrupt config and registration
*/
rxIntrNum = CONFIG_FSI_RX0_INTR1;
status = SemaphoreP_constructBinary(&gFsiRxSemObject, 0);
HwiP_Params_init(&rxHwiPrms);
rxHwiPrms.intNum = rxIntrNum;
rxHwiPrms.callback = Fsi_appRxCallback;
rxHwiPrms.args = (void *) rxBaseAddr;
HwiP_construct(&gFsiRxHwiObject, &rxHwiPrms);
/* Enable RX frame done interrupt */
status += FSI_enableRxInterrupt(rxBaseAddr, FSI_INT1, FSI_RX_EVT_DATA_FRAME);
return status;
}
static void Fsi_appIntrDeInit(uint32_t txBaseAddr, uint32_t rxBaseAddr)
{
/* TX interrupt deinit */
FSI_disableTxInterrupt(txBaseAddr, FSI_INT1, FSI_TX_EVTMASK);
FSI_clearTxEvents(txBaseAddr, FSI_TX_EVTMASK);
HwiP_destruct(&gFsiTxHwiObject);
SemaphoreP_destruct(&gFsiTxSemObject);
/* RX interrupt deinit */
FSI_disableRxInterrupt(rxBaseAddr, FSI_INT1, FSI_TX_EVTMASK);
FSI_clearRxEvents(rxBaseAddr, FSI_RX_EVTMASK);
HwiP_destruct(&gFsiRxHwiObject);
SemaphoreP_destruct(&gFsiRxSemObject);
return;
}

API

APIs for FSI

fsi.h
HwiP_destruct
void HwiP_destruct(HwiP_Object *obj)
Cleanup, delete, destruct a Hwi object.
HwiP_Params
Parameters passed during HwiP_construct.
Definition: HwiP.h:72
FSI_INT1
#define FSI_INT1
Definition: fsi/v0/fsi.h:138
HwiP_construct
int32_t HwiP_construct(HwiP_Object *obj, HwiP_Params *params)
Create a Hwi object.
HwiP_Params_init
void HwiP_Params_init(HwiP_Params *params)
Set default values to HwiP_Params.
FSI_FRAME_TYPE_NWORD_DATA
#define FSI_FRAME_TYPE_NWORD_DATA
Definition: fsi/v0/fsi.h:177
SemaphoreP_destruct
void SemaphoreP_destruct(SemaphoreP_Object *obj)
Cleanup, delete, destruct a semaphore object.
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
HwiP_Params::callback
HwiP_FxnCallback callback
Definition: HwiP.h:75
SemaphoreP_post
void SemaphoreP_post(SemaphoreP_Object *obj)
Post a semaphore object or unlock a mutex.
HwiP_Params::args
void * args
Definition: HwiP.h:76
SemaphoreP_constructBinary
int32_t SemaphoreP_constructBinary(SemaphoreP_Object *obj, uint32_t initValue)
Create a binary semaphore object.
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:159
HwiP_Params::intNum
uint32_t intNum
Definition: HwiP.h:74