PROFINET Device  v1.04.03
PN_API_ETH_SPortDataCheck Struct Reference

#include <PN_API_ETH.h>

Data Fields

uint8_t numberOfPeers
 
PN_API_ETH_SPeerCheck_t aPeers [PN_API_ETH_MAX_PEERS_PER_PORT]
 
bool checkLineDelay
 
uint8_t lineDelayFormat
 
uint32_t lineDelay
 
bool checkMauType
 
uint16_t mauType
 
bool checkLinkState
 
uint8_t linkStateLink
 
uint8_t linkStatePort
 
bool checkSyncDiff
 
uint8_t syncMaster
 
uint8_t cableDelay
 
bool checkMauTypeMode
 
uint8_t mauTypeMode