EtherNet/IP™ Adapter  1.04.01
User Reference Manual
EI_API_ADP_UIntfConf Union Reference

Structure to use as function parameter (attribute parameters) More...

#include <EI_API_def.h>

Data Fields

uint8_t all
 
EI_API_ADP_SIntfConfBits_t bit
 

Detailed Description

Structure to use as function parameter (attribute parameters)