EtherNet/IP™ Adapter  1.04.01
User Reference Manual
EI_API_ADP_INTF_CONF_BITS Struct Reference

General Interface attribute parameter collection. More...

#include <EI_API_def.h>

Data Fields

uint8_t ETHIntfActive: 1
 1 Is the interface activated? More...
 
uint8_t ETHIntfAutoNeg: 1
 2 Is auto neg. on More...
 
uint8_t ETHIntfFDuplex: 1
 3 Is full duplex More...
 
uint8_t ETHIntf100MB: 1
 4 Is 100 mbit More...
 
uint8_t rsvd: 4
 5:8 Reserved More...
 

Detailed Description

General Interface attribute parameter collection.