EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_getHostName()

uint32_t EI_API_ADP_getHostName ( T pAdp_p,
char *  pHostName_p 
)

Get the host name (Instance Attribute ID: 6).

Function that returns a pointer to the host name of the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pHostName_pCharacter array with host name.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char aHostName[65];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getHostName(pEI_API_ADP, aHostName);
See also
EI_API_ADP_setHostName EI_API_ADP_EError_t
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234
EI_API_ADP_getHostName
ETHIP_API uint32_t EI_API_ADP_getHostName(T *pAdp_p, char *pHostName_p)
Get the host name (Instance Attribute ID: 6).
Definition: EI_API_ADP_main.c:3921