EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_setHwSettings()

uint32_t EI_API_ADP_setHwSettings ( T pAdp_p,
bool  hwSettingsEnabled_p,
bool  dhcpEnabled_p 
)

Set the current HW settings.

Let the EtherNet/IP stack know that that the hardware settings are enabled or not. And if so that DHCP is enabled by hardware settings or not.

Parameters
[in]pAdp_pPointer to the adapter.
[in]hwSettingsEnabled_pHardware setting disabled/enabled (0/1).
[in]dhcpEnabled_pDHCP disabled/enabled (0/1).
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_setHwSettings(pEI_API_ADP, true, false);
See also
EI_API_ADP_isHwSettingEnabled EI_API_ADP_EError_t
EI_API_ADP_setHwSettings
ETHIP_API uint32_t EI_API_ADP_setHwSettings(T *pAdp_p, bool hwSettingsEnabled_p, bool dhcpEnabled_p)
Set the current HW settings.
Definition: EI_API_ADP_main.c:5496
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234