EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_getProductName()

uint32_t EI_API_ADP_getProductName ( T pAdp_p,
char *  pProductName_p 
)

Get the adapter Product Name (Instance Attribute ID: 7).

Function that returns a pointer to the product name of the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pProductName_pCharacter array with product name.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char aProductName[33];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getProductName(pEI_API_ADP, aProductName);
See also
EI_API_ADP_setProductName EI_API_ADP_EError_t
EI_API_ADP_getProductName
ETHIP_API uint32_t EI_API_ADP_getProductName(T *pAdp_p, char *pProductName_p)
Get the adapter Product Name (Instance Attribute ID: 7).
Definition: EI_API_ADP_main.c:1601
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234