EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_getDeviceType()

uint32_t EI_API_ADP_getDeviceType ( T pAdp_p,
uint16_t *  pDeviceType_p 
)

Get the adapter Device Type (Instance Attribute ID: 2).

Function that returns the device type of the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pDeviceType_pPointer to the device type.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t deviceType;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getDeviceType(pEI_API_ADP, &deviceType);
See also
EI_API_ADP_setDeviceType EI_API_ADP_EError_t
EI_API_ADP_getDeviceType
ETHIP_API uint32_t EI_API_ADP_getDeviceType(T *pAdp_p, uint16_t *pDeviceType_p)
Get the adapter Device Type (Instance Attribute ID: 2).
Definition: EI_API_ADP_main.c:1060
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234