EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_setProductCode()

uint32_t EI_API_ADP_setProductCode ( T pAdp_p,
uint16_t  productCode_p 
)

Set the adapter Product Code (Instance Attribute ID: 3).

Function that sets the product code of the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[in]productCode_pNew product code.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set product code to 1
errCode = EI_API_ADP_setProductCode(pEI_API_ADP, 0x0001);
See also
EI_API_ADP_getProductCode EI_API_ADP_EError_t
EI_API_ADP_setProductCode
ETHIP_API uint32_t EI_API_ADP_setProductCode(T *pAdp_p, uint16_t productCode_p)
Set the adapter Product Code (Instance Attribute ID: 3).
Definition: EI_API_ADP_main.c:1261
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234