EtherCAT Slave
1.04.06
◆
EC_API_SLV_getOutputProcDataLength()
uint32_t EC_API_SLV_getOutputProcDataLength
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
)
Read the output process data length.
Parameters
[in]
pEcSlaveApi_p
The pointer to the EtherCAT API instance.
Returns
uint32_t Returns the input process data length.
Example
#include <ecSlvApi.h>
uint32_t length =
EC_API_SLV_getOutputProcDataLength
(ptEcSlvApi);
Examples
ESL_cia402Demo.c
.
EC_API_SLV_getOutputProcDataLength
uint32_t EC_API_SLV_getOutputProcDataLength(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
Read the output process data length.
Definition:
ecSlvApi_ProcDataStub.c:674
PDO Configuration
generated by
1.8.18