EtherCAT Slave  1.04.06

◆ EC_SLV_APP_CSV()

void EC_SLV_APP_CSV ( EC_SLV_APP_Sapplication_t pApplication_p,
EC_SLV_API_CiA402_SAxis_t pCiA402Axis_p,
bool  gotOffsets 
)

Cyclic synchronous velocity mode. ETG6010 6.3.

Parameters
[in]ptSlvApiDTK Slave instance.
[in]pCiA402AxisServo Axis description structure.
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
EC_SLV_APP_CSV(S_ecSlvApiHdl, pCiA402Axis);
Examples
ESL_cia402Demo.c.
EC_SLV_API_CiA402_SAxis_t
Data structure to handle an CiA 402 axis.
Definition: ESL_cia402Demo.c:65
EC_SLV_APP_CSV
void EC_SLV_APP_CSV(EC_SLV_APP_Sapplication_t *pApplication_p, EC_SLV_API_CiA402_SAxis_t *pCiA402Axis_p, bool gotOffsets)
Cyclic synchronous velocity mode. ETG6010 6.3.
Definition: ESL_cia402Demo.c:652
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134