Data structure used with MCSPI_transfer()
It indicates how many MCSPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The args variable is an user-definable argument which gets passed to the MCSPI_CallbackFxn when the SPI driver is in MCSPI_TRANSFER_MODE_CALLBACK.
Data Fields | |
uint32_t | channel |
uint32_t | csDisable |
uint32_t | dataSize |
uint32_t | count |
void * | txBuf |
void * | rxBuf |
void * | args |
uint32_t | status |
uint32_t MCSPI_Transaction::channel |
[IN] Channel number (chip select) to use. Valid value from 0 to (MCSPI_MAX_NUM_CHANNELS - 1)
uint32_t MCSPI_Transaction::csDisable |
[IN] TRUE/FALSE to disable CS(chip select)
uint32_t MCSPI_Transaction::dataSize |
[IN] MCSPI data frame size in bits - valid values: 4 bits to 32 bits
The dataSize value determines the element types of txBuf and rxBuf. If the dataSize is from 4 to 8 bits, the driver assumes the data buffers are of type uint8_t (unsigned char). If the dataSize is from 8 to 16 bits, the driver assumes the data buffers are of type uint16_t (unsigned short). If the dataSize is greater than 16 bits, the driver assumes the data buffers are uint32_t (unsigned long).
uint32_t MCSPI_Transaction::count |
[IN] Number of frames for this transaction. This should in word size length and not in bytes
void* MCSPI_Transaction::txBuf |
[IN] void * to a buffer with data to be transmitted.
If txBuf is NULL, the driver sends MCSPI frames with all data set to the default value specified by MCSPI_ChConfig.defaultTxData.
The size of the buffer should be count * MCSPI_Transaction.dataSize in bytes rounded to nearest byte boundary. For example if MCSPI_Transaction.dataSize is 12 bits, then size of buffers should be count * 2 bytes.
void* MCSPI_Transaction::rxBuf |
[IN] void * to a buffer to receive data.
If rxBuf is NULL, the driver discards all MCSPI frames received.
The size of the buffer is similar to txBuf as explained above.
void* MCSPI_Transaction::args |
[IN] Argument to be passed to the callback function
uint32_t MCSPI_Transaction::status |
[OUT] MCSPI_TransferStatus code set by MCSPI_transfer()