Data Fields | |
uint8_t | emacMode |
uint32_t | phyAddr [ICSS_EMAC_MAX_PORTS_PER_INSTANCE] |
uint8_t | phyToMacInterfaceMode |
uint8_t | halfDuplexEnable |
uint8_t | enableIntrPacing |
uint8_t | intrPacingMode |
uint16_t | pacingThreshold |
uint8_t | ethPrioQueue |
uint8_t | learningEnable |
uint8_t | portMask |
uint8_t | txInterruptEnable |
uint32_t | linkIntNum |
uint32_t | rxIntNum |
uint32_t | txIntNum |
uint32_t | l3OcmcBaseAddr |
uint32_t | l3OcmcSize |
uint32_t | linkTaskPriority |
uint32_t | rxTaskPriority |
uint32_t | txTaskPriority |
uint8_t ICSS_EMAC_Attrs::emacMode |
Mode from ICSS_EMAC_Modes
uint32_t ICSS_EMAC_Attrs::phyAddr[ICSS_EMAC_MAX_PORTS_PER_INSTANCE] |
Phy address of the ports. For mac mode, phyAddr[0] is used. For switch mode, phyAddr[0] and phyAddr[1] are used.
uint8_t ICSS_EMAC_Attrs::phyToMacInterfaceMode |
PHY to MAC Interface Mode Valid values : ICSS_EMAC_PhyToMacInterfaceModes
uint8_t ICSS_EMAC_Attrs::halfDuplexEnable |
Flag to enable Half duplex capability. Firmware support also is required to enable the functionality. Valid values : 0 to disable, 1 to enable.
uint8_t ICSS_EMAC_Attrs::enableIntrPacing |
Flag to enable Interrupt pacing. Valid values : ICSS_EMAC_InterruptPacingConfig
uint8_t ICSS_EMAC_Attrs::intrPacingMode |
Pacing mode to be used. Valid values : ICSS_EMAC_InterruptPacingModes
uint16_t ICSS_EMAC_Attrs::pacingThreshold |
Number of packets threshold for Pacing Mode1
uint8_t ICSS_EMAC_Attrs::ethPrioQueue |
Queue Priority separation for RT and NRT packets. If packets are in Queue <= ethPrioQueue, they will be forwarded to RT callback and others to NRT callback
uint8_t ICSS_EMAC_Attrs::learningEnable |
Flag to enable learning. Not applicable for Mac mode. Valid values : ICSS_EMAC_LearningModes
uint8_t ICSS_EMAC_Attrs::portMask |
Port Mask. Indication to LLD which ports to be used Valid values: ICSS_EMAC_MODE_SWITCH, ICSS_EMAC_MODE_MAC1, ICSS_EMAC_MODE_MAC2
uint8_t ICSS_EMAC_Attrs::txInterruptEnable |
Flag to enable TX Interrupt. Valid values : 0 to disable, 1 to enable. If this flag is enabled, ICSS_EMAC_txInterruptHandler() is registered as ISR for the txIntNum interrupt. This interrupt handler unblocks ICSS_EMAC_osTxTaskFnc() and calls the user-specified txCallback.
uint32_t ICSS_EMAC_Attrs::linkIntNum |
uint32_t ICSS_EMAC_Attrs::rxIntNum |
uint32_t ICSS_EMAC_Attrs::txIntNum |
uint32_t ICSS_EMAC_Attrs::l3OcmcBaseAddr |
L3 OCMC Base Address
uint32_t ICSS_EMAC_Attrs::l3OcmcSize |
L3 OCMC Size
uint32_t ICSS_EMAC_Attrs::linkTaskPriority |
Link Task Priority
uint32_t ICSS_EMAC_Attrs::rxTaskPriority |
RX Task Priority
uint32_t ICSS_EMAC_Attrs::txTaskPriority |
TX Task Priority. Valid only if txInterruptEnable is set to 1