This module contains APIs to program and use DMA drivers available in the SoC with UART.
◆ UART_DmaHandle
Handle to the UART DMA Config Object returned by UART_dmaOpen.
◆ UART_dmaOpenFxn
typedef int32_t(* UART_dmaOpenFxn) (UART_Handle uartHandle, void *uartDmaArgs) |
Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
uartHandle | [in] UART Handle |
uartDmaArgs | [in] DMA specific arguments, obtained from the config |
- Returns
- SystemP_SUCCESS on success, else failure
◆ UART_dmaTransferReadFxn
Driver implementation to do a DMA read using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
obj | [in] Pointer to UART object |
transaction | [in] Pointer to UART_Transaction. This parameter can't be NULL |
- Returns
- SystemP_SUCCESS on success, else failure
◆ UART_dmaTransferWriteFxn
Driver implementation to do a DMA write using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
obj | [in] Pointer to UART object |
transaction | [in] Pointer to UART_Transaction. This parameter can't be NULL |
- Returns
- SystemP_SUCCESS on success, else failure
◆ UART_dmaCloseFxn
typedef int32_t(* UART_dmaCloseFxn) (UART_Handle handle) |
Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
handle | [in] UART handle returned from UART_open |
- Returns
- SystemP_SUCCESS on success, else failure
◆ UART_dmaOpen()
API to open an UART DMA channel.
This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig
- Parameters
-
uartHandle | [in] UART Handle |
index | [in] Index of the DMA Config selected for this particular UART driver instance |
- Returns
- Handle to the UART DMA Config Object
◆ UART_dmaClose()
API to close an UART DMA channel.
- Parameters
-
handle | [in] UART handle returned from UART_open |
- Returns
- SystemP_SUCCESS on success, else failure
◆ UART_writeInterruptDma()
API to write data using an UART DMA channel.
- Parameters
-
obj | [in] Pointer to UART object |
transaction | [in] Pointer to UART_Transaction. This parameter can't be NULL |
- Returns
- SystemP_SUCCESS on success, else failure
◆ UART_readInterruptDma()
API to read data using an UART DMA channel.
- Parameters
-
obj | [in] Pointer to UART object |
transaction | [in] Pointer to UART_Transaction. This parameter can't be NULL |
- Returns
- SystemP_SUCCESS on success, else failure