This module contains APIs to program and use the PKA.
|
| file | pka.h |
| | This file contains the prototype of PKA driver APIs.
|
| |
|
| PKA_Handle | PKA_open (uint32_t index) |
| | Function to Open PKA instance, enable PKA engine, Initialize clocks and Load PKA Fw. More...
|
| |
| int32_t | PKA_close (PKA_Handle handle) |
| | Function to close a PKA module specified by the PKA handle. More...
|
| |
| int32_t | PKA_RSAPrivate (PKA_Handle handle, const uint32_t m[PKA_BIGINT_MAX], const struct PKA_RSAPrivkey *k, uint32_t result[PKA_BIGINT_MAX]) |
| | This Function performs Decryption or Signing operations. More...
|
| |
| int32_t | PKA_RSAPublic (PKA_Handle handle, const uint32_t m[PKA_BIGINT_MAX], const struct PKA_RSAPubkey *k, uint32_t result[PKA_BIGINT_MAX]) |
| | This Function performs Encryption or Verification operations. More...
|
| |
| int32_t | PKA_ECDSASign (PKA_Handle handle, const struct PKA_ECPrimeCurveP *cp, const uint32_t priv[PKA_EC_BIGINT_MAX], const uint32_t k[PKA_EC_BIGINT_MAX], const uint32_t h[PKA_EC_BIGINT_MAX], struct PKA_ECDSASig *sig) |
| | ECDSA sign primitive function. More...
|
| |
| int32_t | PKA_ECDSAVerify (PKA_Handle handle, const struct PKA_ECPrimeCurveP *cp, const struct PKA_ECPoint *pub, const struct PKA_ECDSASig *sig, const uint32_t h[PKA_EC_BIGINT_MAX]) |
| | ECDSA verify primitive function. More...
|
| |
◆ PKA_BIGINT_MAX
| #define PKA_BIGINT_MAX (130U) |
Max size of bigint in words - for RSA
◆ PKA_EC_BIGINT_MAX
| #define PKA_EC_BIGINT_MAX (18U) |
Max size of bigint in words - for ECDSA
◆ PKA_EC_PARAM_MAXLEN
| #define PKA_EC_PARAM_MAXLEN (68U) |
Maximum length of a big integer used in EC crypto in bytes, enough to accommodate 521-bit prime curves
◆ PKA_BIGINT_LEN
| #define PKA_BIGINT_LEN |
( |
|
bytelen | ) |
(((bytelen) / 4U) + 1U) |
Length of a biginteger array in words, the +1 is for the size
◆ PKA_RSA_KEY_E_MAXLEN
| #define PKA_RSA_KEY_E_MAXLEN (8U) |
◆ PKA_RSA_KEY_N_MAXLEN
| #define PKA_RSA_KEY_N_MAXLEN (520U) |
◆ PKA_RSA_KEY_PQ_MAXLEN
◆ PKA_RSA_SIG_MAXLEN
◆ PKA_Handle
Handle to the PKA driver.
◆ PKA_open()
Function to Open PKA instance, enable PKA engine, Initialize clocks and Load PKA Fw.
- Returns
- A PKA_Handle on success or a NULL on an error or if it has been opened already
◆ PKA_close()
Function to close a PKA module specified by the PKA handle.
- Parameters
-
◆ PKA_RSAPrivate()
| int32_t PKA_RSAPrivate |
( |
PKA_Handle |
handle, |
|
|
const uint32_t |
m[PKA_BIGINT_MAX], |
|
|
const struct PKA_RSAPrivkey * |
k, |
|
|
uint32_t |
result[PKA_BIGINT_MAX] |
|
) |
| |
This Function performs Decryption or Signing operations.
- Parameters
-
| handle | PKA_Handle returned from PKA_open() |
| m | m value in bigint format. |
| k | RSA private key |
| result | Result of the operation in bigint format. caller must allocate memory size of (2 * sizeof(p)) for the result. |
- Returns
- SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.
◆ PKA_RSAPublic()
| int32_t PKA_RSAPublic |
( |
PKA_Handle |
handle, |
|
|
const uint32_t |
m[PKA_BIGINT_MAX], |
|
|
const struct PKA_RSAPubkey * |
k, |
|
|
uint32_t |
result[PKA_BIGINT_MAX] |
|
) |
| |
This Function performs Encryption or Verification operations.
- Parameters
-
| handle | PKA_Handle returned from PKA_open() |
| m | m value in bigint format. |
| k | RSA public key |
| result | Result of the operation in bigint format. caller must allocate the same memory as s and n for this array. |
- Returns
- SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.
◆ PKA_ECDSASign()
| int32_t PKA_ECDSASign |
( |
PKA_Handle |
handle, |
|
|
const struct PKA_ECPrimeCurveP * |
cp, |
|
|
const uint32_t |
priv[PKA_EC_BIGINT_MAX], |
|
|
const uint32_t |
k[PKA_EC_BIGINT_MAX], |
|
|
const uint32_t |
h[PKA_EC_BIGINT_MAX], |
|
|
struct PKA_ECDSASig * |
sig |
|
) |
| |
ECDSA sign primitive function.
- Parameters
-
| handle | PKA_Handle returned from PKA_open() |
| cp | EC curve parameters |
| priv | EC private key |
| k | Random number for each signing |
| h | Hash value of message to sign in bigint format |
| sig | ECDSA Signature - 'r' and 's' values |
- Returns
- SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.
◆ PKA_ECDSAVerify()
ECDSA verify primitive function.
- Parameters
-
| handle | PKA_Handle returned from PKA_open() |
| cp | EC curve parameters |
| pub | EC Public key |
| sig | ECDSA Signature - 'r' & 's' value in bigint format |
| h | Hash value of message to verify in bigint format |
- Returns
- SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.
◆ gPkaConfig
Externally defined driver configuration array.
◆ gPkaConfigNum
Externally defined driver configuration Num.