AM64x MCU+ SDK  08.02.00
enet_cfg.h File Reference

Introduction

This file contains the Enet configuration parameters.

Go to the source code of this file.

Macros

#define ENET_ON   (1U)
 Build-time config option is enabled. More...
 
#define ENET_OFF   (0U)
 Build-time config option is disabled. More...
 
#define ENET_CFG_IS_ON(name)   ((ENET_CFG_ ## name) == ENET_ON)
 Preprocessor check if config option is enabled. More...
 
#define ENET_CFG_IS_OFF(name)   ((ENET_CFG_ ## name) == ENET_OFF)
 Preprocessor check if config option is disabled. More...
 
#define ENET_CFG_PRINT_BUF_LEN   (200U)
 EnetUtils print buffer length. More...
 
#define ENET_CFG_HAS_DEFAULT_OSAL   (ENET_ON)
 Whether Enet driver has a default OSAL implementation. More...
 
#define ENET_CFG_HAS_DEFAULT_UTILS   (ENET_ON)
 Whether Enet driver has a default utils implementation. More...
 
#define ENET_CFG_SANITY_CHECKS   (ENET_ON)
 Enable top-layer sanity checks and misc debug info. More...
 
#define ENET_CFG_ENETPHY_PHY_MAX   (13U)
 Maximum number of supported PHYs (allocated PHY objects). More...
 
#define ENET_CFG_CPSW_SGMII   (ENET_ON)
 CPSW Q/SGMII support (requires ENET_CFG_CPSW_MACPORT_SGMII). More...
 
#define ENET_CFG_CPSW_INTERVLAN   (ENET_ON)
 CPSW interVLAN support support (requires ENET_CFG_CPSW_MACPORT_INTERVLAN). More...
 
#define ENET_CFG_MDIO_CLAUSE45   (ENET_ON)
 MDIO Clause-45 frame support. More...
 
#define ENET_CFG_CPSW_HOSTPORT_TRAFFIC_SHAPING   (ENET_ON)
 
#define ENET_CFG_CPSW_MACPORT_SGMII   (ENET_ON)
 
#define ENET_CFG_CPSW_MACPORT_INTERVLAN   (ENET_ON)
 
#define ENET_CFG_CPSW_CPTS_STATS   (ENET_ON)
 
#define ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE   (128U)
 
#define ENET_CFG_REMOTE_CLIENT_CORES_MAX   (6U)
 Maximum number of client core that the Enet driver can serve. More...
 
#define ENET_CFG_RM_MAC_ADDR_MAX   (10U)
 Maximum number of MAC addresses that Enet RM can manage. More...
 
#define ENET_CFG_RM_TX_CH_MAX   (8U)
 Maximum number of TX channels that Enet RM can manage. More...
 
#define ENET_CFG_RM_RX_CH_MAX   (64U)
 Maximum number of RX channels that Enet RM can manage. More...
 
#define ENET_CFG_TX_CHANNELS_NUM   (8U)
 SOC specific configuration defines. More...
 
#define ENET_CFG_RX_FLOWS_NUM   (8U)
 
#define ENET_CFG_RING_MON_NUM   (4U)
 

Macro Definition Documentation

◆ ENET_ON

#define ENET_ON   (1U)

Build-time config option is enabled.

◆ ENET_OFF

#define ENET_OFF   (0U)

Build-time config option is disabled.

◆ ENET_CFG_IS_ON

#define ENET_CFG_IS_ON (   name)    ((ENET_CFG_ ## name) == ENET_ON)

Preprocessor check if config option is enabled.

◆ ENET_CFG_IS_OFF

#define ENET_CFG_IS_OFF (   name)    ((ENET_CFG_ ## name) == ENET_OFF)

Preprocessor check if config option is disabled.

◆ ENET_CFG_PRINT_BUF_LEN

#define ENET_CFG_PRINT_BUF_LEN   (200U)

EnetUtils print buffer length.

◆ ENET_CFG_HAS_DEFAULT_OSAL

#define ENET_CFG_HAS_DEFAULT_OSAL   (ENET_ON)

Whether Enet driver has a default OSAL implementation.

◆ ENET_CFG_HAS_DEFAULT_UTILS

#define ENET_CFG_HAS_DEFAULT_UTILS   (ENET_ON)

Whether Enet driver has a default utils implementation.

◆ ENET_CFG_SANITY_CHECKS

#define ENET_CFG_SANITY_CHECKS   (ENET_ON)

Enable top-layer sanity checks and misc debug info.

◆ ENET_CFG_ENETPHY_PHY_MAX

#define ENET_CFG_ENETPHY_PHY_MAX   (13U)

Maximum number of supported PHYs (allocated PHY objects).

◆ ENET_CFG_CPSW_SGMII

#define ENET_CFG_CPSW_SGMII   (ENET_ON)

CPSW Q/SGMII support (requires ENET_CFG_CPSW_MACPORT_SGMII).

◆ ENET_CFG_CPSW_INTERVLAN

#define ENET_CFG_CPSW_INTERVLAN   (ENET_ON)

CPSW interVLAN support support (requires ENET_CFG_CPSW_MACPORT_INTERVLAN).

◆ ENET_CFG_MDIO_CLAUSE45

#define ENET_CFG_MDIO_CLAUSE45   (ENET_ON)

MDIO Clause-45 frame support.

◆ ENET_CFG_CPSW_HOSTPORT_TRAFFIC_SHAPING

#define ENET_CFG_CPSW_HOSTPORT_TRAFFIC_SHAPING   (ENET_ON)

◆ ENET_CFG_CPSW_MACPORT_SGMII

#define ENET_CFG_CPSW_MACPORT_SGMII   (ENET_ON)

◆ ENET_CFG_CPSW_MACPORT_INTERVLAN

#define ENET_CFG_CPSW_MACPORT_INTERVLAN   (ENET_ON)

◆ ENET_CFG_CPSW_CPTS_STATS

#define ENET_CFG_CPSW_CPTS_STATS   (ENET_ON)

◆ ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE

#define ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE   (128U)

◆ ENET_CFG_REMOTE_CLIENT_CORES_MAX

#define ENET_CFG_REMOTE_CLIENT_CORES_MAX   (6U)

Maximum number of client core that the Enet driver can serve.

◆ ENET_CFG_RM_MAC_ADDR_MAX

#define ENET_CFG_RM_MAC_ADDR_MAX   (10U)

Maximum number of MAC addresses that Enet RM can manage.

◆ ENET_CFG_RM_TX_CH_MAX

#define ENET_CFG_RM_TX_CH_MAX   (8U)

Maximum number of TX channels that Enet RM can manage.

◆ ENET_CFG_RM_RX_CH_MAX

#define ENET_CFG_RM_RX_CH_MAX   (64U)

Maximum number of RX channels that Enet RM can manage.

◆ ENET_CFG_TX_CHANNELS_NUM

#define ENET_CFG_TX_CHANNELS_NUM   (8U)

SOC specific configuration defines.

◆ ENET_CFG_RX_FLOWS_NUM

#define ENET_CFG_RX_FLOWS_NUM   (8U)

◆ ENET_CFG_RING_MON_NUM

#define ENET_CFG_RING_MON_NUM   (4U)