AM64x MCU+ SDK  08.02.00
core Directory Reference

Files

file  enet_base.h [code]
 This file contains the type definitions and helper macros for the Enet Peripheral interface.
 
file  enet_dma.h [code]
 This file contains the type definitions and helper macros for the Enet Data Path (DMA) interface.
 
file  enet_dma_pktutils.h [code]
 Enet DMA utility API to check packet and descriptor ownership states during development and debug.
 
file  enet_ioctl.h [code]
 This file contains the type definitions and helper macros for the Enet IOCTL interface.
 
file  enet_mod.h [code]
 This file contains the type definitions and helper macros for the Enet Module interface.
 
file  enet_mod_fdb.h [code]
 This file contains the type definitions and helper macros for the Enet Forwarding Database (FDB) module interface.
 
file  enet_mod_hostport.h [code]
 This file contains the type definitions and helper macros for the Enet Hostport module interface.
 
file  enet_mod_macport.h [code]
 This file contains the type definitions and helper macros for the Enet MAC port module interface.
 
file  enet_mod_mdio.h [code]
 This file contains the type definitions and helper macros for the Enet MDIO module.
 
file  enet_mod_phy.h [code]
 This file contains the type definitions and helper macros for the Ethernet PHY interface.
 
file  enet_mod_port.h [code]
 This file contains the type definitions and helper macros that are common for host and MAC ports.
 
file  enet_mod_stats.h [code]
 This file contains the type definitions and helper macros for the Enet Statistics module interface.
 
file  enet_mod_timesync.h [code]
 This file contains the type definitions and helper macros for the Enet Time Synchronization module interface.
 
file  enet_osal.h [code]
 This file contains the OSAL API of the Enet driver.
 
file  enet_per.h [code]
 This file contains the type definitions and helper macros for the Enet Peripheral interface.
 
file  enet_queue.h [code]
 This file contains the type definitions and helper macros for the Enet software queue.
 
file  enet_rm.h [code]
 This file contains the type definitions and helper macros for the Enet Resource Manager module.
 
file  enet_soc.h [code]
 This file contains the type definitions and helper macros for the Enet SoC interface.
 
file  enet_trace.h [code]
 This file contains the type definitions and helper macros for the Enet Trace interface.
 
file  enet_types.h [code]
 This file contains the basic types using across the Enet driver.
 
file  enet_utils.h [code]
 This file contains the type definitions and function prototypes of the Enet Utils functionality.