| uint32_t EI_API_CIP_createClass | ( | T * | pCipNode_p, |
| uint16_t | classId_p | ||
| ) |
Create a CIP class.
This function creates a CIP class. The class identifier is specified in parameter classId.
| [in] | pCipNode_p | Pointer to the CIP node. |
| [in] | classId_p | Class identifier. |
| EI_API_CIP_eERR_OK | Success. |
| EI_API_CIP_eERR_NODE_INVALID | CIP node is invalid, possibly EI_API_CIP_NODE_new() was not called. |
| EI_API_CIP_eERR_DICTIONARY_FULL | CIP dictionary is full, no more class or instance can be added. |
| EI_API_CIP_eERR_CLASS_ALREADY_EXIST | Class already exists in CIP node dictionary. |
| EI_API_CIP_eERR_MEMALLOC | Memory allocation error. |
| EI_API_CIP_eERR_INSTANCE_UNKNOWN_STATE | Unknown state during class operation reached. |