PROFINET Device  v1.04.02

◆ PN_API_IM_removeImCarrier()

uint32_t PN_API_IM_removeImCarrier ( PN_API_IM_SCarrierAddress_t pAddress_p)

Remove an I&M carrier from stack.

With this function application removes an I&M carrier from the stack. Concerned submodule has no attached I&M data anymore.

Remarks
User shall concern that a device must always have a device representative. In case of removing current device representative, user must add a new one and take care of data consistency (Chassis Id, RPC Annotation...).
Warning
If a real submodule is being pulled using PN_API_DEV_APP_pullSubmodule(), attached I&M carrier (if available) will be removed as well.
Parameters
[in]pAddress_pAddress of I&M carrier, which is being removed.
Returns
PN_API_IM_EError_t as uint32_t value.
Return values
PN_API_IM_eOKFunction successful.
PN_API_IM_eERR_REMOVE_IM_INVALID_POINTERInvalid parameters (NULL pointers).
PN_API_IM_eERR_REMOVE_IM_CARRIER_NOT_EXISTSpecified I&M carrier does not exist.
Example
#include <PN_API_IM.h>
//New instance of I&M Carrier.
//Fill address.
address.api = XXX;
address.slotNum = YYY;
address.subslotNum = ZZZ;
//Remove I&M carrier and analyze result.
uint32_t result = PN_API_IM_removeImCarrier(&address)
if (result == PN_API_IM_eOK) // success
PN_API_IM_removeImCarrier
uint32_t PN_API_IM_removeImCarrier(PN_API_IM_SCarrierAddress_t *pAddress_p)
Remove an I&M carrier from stack.
Definition: PN_API_main.c:1484
PN_API_IM_SCarrierAddress::subslotNum
uint16_t subslotNum
Definition: PN_API_IM.h:271
PN_API_IM_eOK
@ PN_API_IM_eOK
Definition: PN_API_IM.h:76
PN_API_IM_SCarrierAddress::api
uint32_t api
Definition: PN_API_IM.h:269
PN_API_IM_SCarrierAddress::slotNum
uint16_t slotNum
Definition: PN_API_IM.h:270
PN_API_IM_SCarrierAddress
Definition: PN_API_IM.h:268