IO-Link Master  1.05.01
SMI On Request Data

Overview

SMI On Request Data.

Typedefs

typedef void(* IOLM_SMI_CBDeviceWriteCnf) (INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16Error_p)
 Set Device On-request Data confirmation callback. More...
 
typedef void(* IOLM_SMI_CBDeviceReadCnf) (INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16Error_p, INT16U u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
 Get Device On-request Data confirmation callback. More...
 

Functions

IOL_FUNC_DECL void IOLM_SMI_vDeviceWriteReq (INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
 Set Device On-request Data. More...
 
IOL_FUNC_DECL void IOLM_SMI_vDeviceReadReq (INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
 Get Device On-request Data. More...
 

Typedef Documentation

◆ IOLM_SMI_CBDeviceReadCnf

IOLM_SMI_CBDeviceReadCnf

Get Device On-request Data confirmation callback.

This service allows for reading On-request Data (OD) from the Device via the Master. Confirmation to the IOLM_SMI_vDeviceReadReq request.

Parameters
[in]u8ClientID_pClient ID.
[in]u8Port_pPort ID.
[in]u16Error_pError message as IOL_EErrorType.
[in]u16ArgBlockLength_pLength of ArgBlock.
[in]pu8ArgBlock_pData pointer which points to the Device On-request Data (IOLM_SMI_SOnRequestData).
Example
void IOLM_SMI_vDeviceReadCnf(INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16Error_p,
INT16U u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
{
if (u16Error_p != IOL_eErrorType_NONE)
{
UART_printf("IO-Link port %u: Read failed with error 0x%04x\n", u8Port_p, u16Error_p);
}
else
{
// ToDo: Insert application specific code here
}
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

◆ IOLM_SMI_CBDeviceWriteCnf

IOLM_SMI_CBDeviceWriteCnf

Set Device On-request Data confirmation callback.

This callback indicates an answer to an On-request Data (OD) write request from a Device. Confirmation to the IOLM_SMI_vDeviceWriteReq request.

Parameters
[in]u8ClientID_pClient ID.
[in]u8Port_pPort ID.
[in]u16Error_pError message as IOL_EErrorType.
Example
void IOLM_SMI_vDeviceWriteCnf(INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16Error_p)
{
if (u16Error_p != IOL_eErrorType_NONE)
{
UART_printf("IO-Link port %u: Write failed with error 0x%04x\n", u8Port_p, u16Error_p);
}
else
{
// ToDo: Insert application specific code here
}
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

Function Documentation

◆ IOLM_SMI_vDeviceReadReq()

IOL_FUNC_DECL void IOLM_SMI_vDeviceReadReq ( INT8U  u8ClientID_p,
INT8U  u8Port_p,
INT16U  u16ArgBlockLength_p,
INT8U pu8ArgBlock_p 
)

Get Device On-request Data.

This service allows for reading On-request Data (OD) from the Device via the Master. The answer to the request is the function IOLM_SMI_CBDeviceReadCnf.

Parameters
[in]u8ClientID_pClient ID.
[in]u8Port_pPort ID.
[in]u16ArgBlockLength_pLength of ArgBlock.
[in]pu8ArgBlock_pData pointer which points to the Device On-request Data (IOLM_SMI_SOnRequestData).
Example
INT8U au8Mem[IOLM_SMI_ARGBLOCK_ONREQ_LEN(0)]; // Allocate ArgBlock memory
// Fill request
psuReq->u16ArgBlockID = IOLM_SMI_ENDIAN_16(IOLM_SMI_eArgBlockID_OnRequestDataRead);
psuReq->u16Index = IOLM_SMI_ENDIAN_16(16); // Index 16 = VendorName
psuReq->u8Subindex = 0;
// Send request
0, // Client ID
0, // Port
IOLM_SMI_ARGBLOCK_ONREQ_LEN(0), // Length
au8Mem
);
// Wait for IOLM_SMI_CBDeviceReadCnf

◆ IOLM_SMI_vDeviceWriteReq()

IOL_FUNC_DECL void IOLM_SMI_vDeviceWriteReq ( INT8U  u8ClientID_p,
INT8U  u8Port_p,
INT16U  u16ArgBlockLength_p,
INT8U pu8ArgBlock_p 
)

Set Device On-request Data.

This service allows for writing On-request Data (OD) for propagation to the Device. The answer to the request is the function IOLM_SMI_CBDeviceWriteCnf.

Parameters
[in]u8ClientID_pClient ID.
[in]u8Port_pPort ID.
[in]u16ArgBlockLength_pLength of ArgBlock.
[in]pu8ArgBlock_pData pointer which points to the Device's On-request Data (IOLM_SMI_SOnRequestData).
Example
INT8U au8Mem[IOLM_SMI_ARGBLOCK_ONREQ_LEN(2)]; // Allocate ArgBlock memory
// Fill request
psuReq->u16ArgBlockID = IOLM_SMI_ENDIAN_16(IOLM_SMI_eArgBlockID_OnRequestDataWrite);
psuReq->u16Index = IOLM_SMI_ENDIAN_16(123); // Index
psuReq->u8Subindex = 0; // SubIndex
psuReq->au8Data[0] = 0x12; // Data
psuReq->au8Data[1] = 0x34; // Data
// Send request
0, // Client ID
0, // Port
IOLM_SMI_ARGBLOCK_ONREQ_LEN(2), // Length
au8Mem
);
// Wait for IOLM_SMI_CBDeviceWriteCnf
IOLM_SMI_vDeviceWriteReq
void IOLM_SMI_vDeviceWriteReq(INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
Set Device On-request Data.
Definition: IOLM_SMI.c:3019
IOLM_SMI_SOnRequestData::u16Index
INT16U u16Index
Big endian.
Definition: IOLM_SMI_Types.h:762
IOLM_SMI_vDeviceReadReq
void IOLM_SMI_vDeviceReadReq(INT8U u8ClientID_p, INT8U u8Port_p, INT16U u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
Get Device On-request Data.
Definition: IOLM_SMI.c:3031
IOLM_SMI_SOnRequestData
This structure is used for On-request Data.
Definition: IOLM_SMI_Types.h:760
INT16U
uint16_t INT16U
16 bit unsigned integer
Definition: IOL_Port_Types.h:70
IOLM_SMI_SOnRequestData::u16ArgBlockID
INT16U u16ArgBlockID
Big endian.
Definition: IOLM_SMI_Types.h:761
IOL_eErrorType_NONE
@ IOL_eErrorType_NONE
No error.
Definition: IOL_Types.h:543
INT8U
uint8_t INT8U
8 bit unsigned integer
Definition: IOL_Port_Types.h:68