EtherNet/IP™ Adapter  1.04.00
User Reference Manual
EI_API_ADP_SRevision Struct Reference

#include <EI_API_ADP.h>

Data Fields

uint8_t major
 
uint8_t minor
 

Detailed Description

The Revision attribute, which consists of Major and Minor Revisions, identifies the Revision of the item the Identity Object is representing. The value zero is not valid for either the Major or Minor Revision fields. If the Device Type of the instance is Embedded Component (0xC8), the Major Revision and/or Minor Revision may be zero.

Examples
App.c.