EtherNet/IP™ Adapter  1.04.00
User Reference Manual

◆ EI_API_ADP_setEnipAcdAddr()

uint32_t EI_API_ADP_setEnipAcdAddr ( T *  pAdp_p,
const EI_API_ADP_SParam_t pEnipAcdAddr_p 
)

Set the address conflict detection MAC address (Instance Attribute ID: 11).

Function that sets the MAC address of the last address conflict detected by the Address Conflict Detection (ACD).

Parameters
[in]pAdp_pPointer to the adapter.
[in]pEnipAcdAddr_pPointer to the Ethernet Address Conflict Detection MAC address packed within a EI_API_ADP_SParam_t type.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
EI_API_ADP_eERR_LENGTHIllegal parameter length.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t macAddr[] = { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 };
EI_API_ADP_SParam_t macAcd = { 6, macAddr };
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// clear ACD MAC address
errCode = EI_API_ADP_setEnipAcdAddr(pEI_API_ADP, macAcd);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
ETHIP_API uint32_t EI_API_ADP_setEnipAcdAddr(T *pAdp_p, const EI_API_ADP_SParam_t *pEnipAcdAddr_p)
Set the address conflict detection MAC address (Instance Attribute ID: 11).
Definition: EI_API_ADP_main.c:3189
Definition: EI_API_ADP.h:113
See also
EI_API_ADP_getEnipAcdAddr EI_API_ADP_SParam_t EI_API_ADP_EError_t