EtherNet/IP™ Adapter  1.04.00
User Reference Manual

◆ EI_API_ADP_getProductCode()

uint32_t EI_API_ADP_getProductCode ( T *  pAdp_p,
uint16_t *  pProductCode_p 
)

Get the adapter product code (Instance Attribute ID: 3).

Function that returns the product code of the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pProductCode_pPointer to the product code.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t productCode;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getProductCode(pEI_API_ADP, &productCode);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
ETHIP_API uint32_t EI_API_ADP_getProductCode(T *pAdp_p, uint16_t *pProductCode_p)
Get the adapter product code (Instance Attribute ID: 3).
Definition: EI_API_ADP_main.c:1195
See also
EI_API_ADP_setProductCode EI_API_ADP_EError_t