EtherNet/IP™ Adapter  1.04.00
User Reference Manual

◆ EI_API_ADP_delete()

uint32_t EI_API_ADP_delete ( T *  pAdp_p)

Delete an existing EtherNet/IP adapter.

If an adapter was created it can be deleted with this function. The memory which was allocated by the adapter will be freed.

Parameters
[in]pAdp_pPointer to the adapter.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
// Create a new adapter
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
...
// Delete the adapter
errCode = EI_API_ADP_delete(pEI_API_ADP);
ETHIP_API uint32_t EI_API_ADP_delete(T *pAdp_p)
Delete an existing EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:345
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
See also
EI_API_ADP_new EI_API_ADP_EError_t