AM64x MCU+ SDK  08.01.00
superConfig Struct Reference

Detailed Description

Supervisor configuration. Attribute ID 4.

Data Fields

uint8_t superEnable
 
uint32_t beaconInterval
 
uint32_t beaconTimeout
 
uint16_t vLanId
 
uint8_t supPrecedence
 

Field Documentation

◆ superEnable

uint8_t superConfig::superEnable

device configured to run as supervisor default : false

◆ beaconInterval

uint32_t superConfig::beaconInterval

beacon interval value (microseconds)

◆ beaconTimeout

uint32_t superConfig::beaconTimeout

beacon timeout value (microseconds)

◆ vLanId

uint16_t superConfig::vLanId

VLAN Id

◆ supPrecedence

uint8_t superConfig::supPrecedence

Supervisor precedence