AM64x MCU+ SDK  08.01.00
ICSS_EMAC_CallBackObject Struct Reference

Detailed Description

Different callbacks which can be registered.
While calling the function set in ICSS_EMAC_CallBack, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (as mentioned in the member descriptions), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig.

Data Fields

ICSS_EMAC_CallBackConfig port0LinkCallBack
 
ICSS_EMAC_CallBackConfig port1LinkCallBack
 
ICSS_EMAC_CallBackConfig rxNRTCallBack
 
ICSS_EMAC_CallBackConfig rxRTCallBack
 
ICSS_EMAC_CallBackConfig txCallBack
 
ICSS_EMAC_CallBackConfig learningExCallBack
 

Field Documentation

◆ port0LinkCallBack

ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::port0LinkCallBack

Callback function for link change on Port 0. Second argument to callback is linkStatus

◆ port1LinkCallBack

ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::port1LinkCallBack

Callback function for link change on Port 1. Second argument to callback is linkStatus

◆ rxNRTCallBack

ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::rxNRTCallBack

Callback function for packets received with queueNumber >= ethPrioQueue (of ICSS_EMAC_Attrs). Second argument to callback is queueNumber.

◆ rxRTCallBack

ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::rxRTCallBack

Callback function for packets received with queueNumber < ethPrioQueue (of ICSS_EMAC_Attrs). Second argument to callback is queueNumber.

◆ txCallBack

ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::txCallBack

Callback function for packet Tx completion. Second argument is NULL

◆ learningExCallBack

ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::learningExCallBack

Callback function for protocol specific exception adaptation in learning. Second argument is macId