Structure holding the dead band generation sub-module configuration parameters.
Data Fields | |
uint32_t | inputMode |
uint32_t | outputMode |
uint32_t | polaritySelect |
uint32_t | risingEdgeDelay |
uint32_t | fallingEdgeDelay |
uint32_t Epwm_DeadbandCfg_t::inputMode |
Input mode control that selects the input source to the falling-edge and rising-edge delay. This can take values from the following enum Epwm_DbInMode_t.
uint32_t Epwm_DeadbandCfg_t::outputMode |
Output mode control that selectively enable or bypass the dead-band generation for the falling-edge and rising-edge delay. This can take values from the following enum Epwm_DbOutMode_t.
uint32_t Epwm_DeadbandCfg_t::polaritySelect |
Polarity selection control that allows selectively invert one of the delayed signals before it is sent out of the dead-band sub-module. This can take values from the following enum Epwm_DbPolSel_t.
uint32_t Epwm_DeadbandCfg_t::risingEdgeDelay |
Rising edge delay count in cycles.
uint32_t Epwm_DeadbandCfg_t::fallingEdgeDelay |
Falling edge delay count in cycles.