Structure holding the configuration parameters of Chopper sub-module.
Data Fields | |
uint32_t | dutyCycle |
uint32_t | clkFrequency |
uint32_t | oneShotPulseWidth |
uint32_t Epwm_ChopperCfg_t::dutyCycle |
Chopping clock duty cycle. This can take values from the following enum Epwm_ChpDutyCycle_t.
uint32_t Epwm_ChopperCfg_t::clkFrequency |
Chopping clock frequency. This can take values from the following enum Epwm_ChpClkFreq_t.
uint32_t Epwm_ChopperCfg_t::oneShotPulseWidth |
One shot pulse width: pulse width of first pulse. This can take values from the following enum Epwm_ChpOshtWidth_t.