AM64x MCU+ SDK  08.01.00
EnetRm_MacAddressPool Struct Reference

Detailed Description

Enet RM MAC address pool.

This structure has the pool of MAC addresses that are being managed.

Data Fields

uint32_t numMacAddress
 
uint8_t macAddress [ENET_RM_NUM_MACADDR_MAX][ENET_MAC_ADDR_LEN]
 

Field Documentation

◆ numMacAddress

uint32_t EnetRm_MacAddressPool::numMacAddress

Number of MAC addresses

◆ macAddress

uint8_t EnetRm_MacAddressPool::macAddress[ENET_RM_NUM_MACADDR_MAX][ENET_MAC_ADDR_LEN]

Array of MAC addresses, not to exceed ENET_RM_NUM_MACADDR_MAX