AM64x MCU+ SDK  08.01.00
Cpsw_Cfg Struct Reference

Detailed Description

CPSW configuration.

Configuration information for the CPSW driver.

Data Fields

uint32_t escalatePriorityLoadVal
 
const void * dmaCfg
 
Cpsw_VlanCfg vlanCfg
 
uint32_t txMtu [ENET_PRI_NUM]
 
CpswHostPort_Cfg hostPortCfg
 
CpswAle_Cfg aleCfg
 
CpswCpts_Cfg cptsCfg
 
Mdio_Cfg mdioCfg
 
EnetRm_ResCfg resCfg
 
uint32_t intrPriority
 
Cpsw_MdioLinkStateChangeCb mdioLinkStateChangeCb
 
void * mdioLinkStateChangeCbArg
 
Cpsw_PortLinkStatusChangeCb portLinkStatusChangeCb
 
void * portLinkStatusChangeCbArg
 
bool enableQsgmii0RDC
 
bool enableQsgmii1RDC
 

Field Documentation

◆ escalatePriorityLoadVal

uint32_t Cpsw_Cfg::escalatePriorityLoadVal

Escalate priority load value

◆ dmaCfg

const void* Cpsw_Cfg::dmaCfg

Configuration of the CPSW DMA

◆ vlanCfg

Cpsw_VlanCfg Cpsw_Cfg::vlanCfg

VLAN configuration (inner/outer VLAN ltype, customer/service switch)

◆ txMtu

uint32_t Cpsw_Cfg::txMtu[ENET_PRI_NUM]

Max packet length transmitted on egress. Packets that are larger than this length will be dropped. This length excludes VLAN addition or removal

◆ hostPortCfg

CpswHostPort_Cfg Cpsw_Cfg::hostPortCfg

Configuration of the CPSW DMA *‍/ EnetDma_Cfg dmaCfg;

/*! Configuration of the host (CPPI) port 

◆ aleCfg

CpswAle_Cfg Cpsw_Cfg::aleCfg

Configure of the ALE module

◆ cptsCfg

CpswCpts_Cfg Cpsw_Cfg::cptsCfg

Configure of the CPTS module

◆ mdioCfg

Mdio_Cfg Cpsw_Cfg::mdioCfg

Configuration of the MDIO module

◆ resCfg

EnetRm_ResCfg Cpsw_Cfg::resCfg

Configuration of CPSW Resource Partition

◆ intrPriority

uint32_t Cpsw_Cfg::intrPriority

Interrupt priority

◆ mdioLinkStateChangeCb

Cpsw_MdioLinkStateChangeCb Cpsw_Cfg::mdioLinkStateChangeCb

MDIO Link state change callback function pointer

◆ mdioLinkStateChangeCbArg

void* Cpsw_Cfg::mdioLinkStateChangeCbArg

Application data to be passed to the MDIO link state change callback

◆ portLinkStatusChangeCb

Cpsw_PortLinkStatusChangeCb Cpsw_Cfg::portLinkStatusChangeCb

Port link status change callback function pointer. This callback is called when the port link is either fully functional or fully shutdown

◆ portLinkStatusChangeCbArg

void* Cpsw_Cfg::portLinkStatusChangeCbArg

Application data to be passed to the port link status change callback

◆ enableQsgmii0RDC

bool Cpsw_Cfg::enableQsgmii0RDC

QSGMII0 Running Disparity Check (RDCD) enable - disables the rx running disparity so that errors do not propagate across lanes. It can be used when debugging a multi-port link to disable the disparity to isolate the receive errors

◆ enableQsgmii1RDC

bool Cpsw_Cfg::enableQsgmii1RDC

QSGMII1 Running Disparity Check (RDCD) enable