AM64x MCU+ SDK  08.01.00

Detailed Description

Input args for CPSW_ALE_IOCTL_SET_TRUNK_CFG command.

Data Fields

uint32_t trunkId
 
uint32_t numPorts
 
uint32_t trunkPortIdx [CPSW_ALE_NUM_PORTS]
 
uint32_t trunkHashBase
 
bool dstIPEn
 
bool srcIPEn
 
bool innerVlanEn
 
bool enablePri
 
bool srcEn
 
bool dstEnEn
 

Field Documentation

◆ trunkId

uint32_t CpswAle_TrunkCfg::trunkId

Trunk group ID value

◆ numPorts

uint32_t CpswAle_TrunkCfg::numPorts

Number of ports in the trunk group

◆ trunkPortIdx

uint32_t CpswAle_TrunkCfg::trunkPortIdx[CPSW_ALE_NUM_PORTS]

Trunk group index value

◆ trunkHashBase

uint32_t CpswAle_TrunkCfg::trunkHashBase

Hash formula starting value

◆ dstIPEn

bool CpswAle_TrunkCfg::dstIPEn

Enables the destination MAC address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination

◆ srcIPEn

bool CpswAle_TrunkCfg::srcIPEn

Enables the source MAC address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination

◆ innerVlanEn

bool CpswAle_TrunkCfg::innerVlanEn

Enables the inner VLAN ID value (C-VLANID) to be used with the hash function G(X) = 1 + X+ X^3 and affects the trunk port transmit link determination

◆ enablePri

bool CpswAle_TrunkCfg::enablePri

Enables the VLAN Priority bits to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination

◆ srcEn

bool CpswAle_TrunkCfg::srcEn

Enables the source IP address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination

◆ dstEnEn

bool CpswAle_TrunkCfg::dstEnEn

Enables the destination IP address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination