AM64x MCU+ SDK  08.01.00
CpswAle_SetBcastMcastRateLimitInArgs Struct Reference

Detailed Description

Input args for CPSW_ALE_IOCTL_SET_BCAST_MCAST_LIMIT command.

Data Fields

bool rateLimitAtTxPort
 
uint32_t numPorts
 
CpswAle_PortBcastMcastRateLimitParams portPrms [CPSW_ALE_NUM_PORTS]
 

Field Documentation

◆ rateLimitAtTxPort

bool CpswAle_SetBcastMcastRateLimitInArgs::rateLimitAtTxPort

Rate limit to be done at transmit or receive port

◆ numPorts

uint32_t CpswAle_SetBcastMcastRateLimitInArgs::numPorts

Number of port for which broadcast/multicast rate limiting config to be applied

◆ portPrms

CpswAle_PortBcastMcastRateLimitParams CpswAle_SetBcastMcastRateLimitInArgs::portPrms[CPSW_ALE_NUM_PORTS]

Per port broadcast/multicast rate limit params