AM64x MCU+ SDK  08.01.00
flash.h File Reference

Go to the source code of this file.

Data Structures

struct  Flash_Params
 Parameters passed during Flash_open() More...
 
struct  Flash_Fxns
 Driver implementation callbacks. More...
 
struct  Flash_Attrs
 Flash device attributes, these are filled by SysCfg based on the flash device that is selected. More...
 
struct  Flash_Config
 Flash driver configuration, these are filled by SysCfg based on the flash device that is selected. More...
 

Typedefs

typedef void * Flash_Handle
 Handle to the FLash driver returned by Flash_opem() More...
 
typedef struct Flash_Config_s Flash_Config
 Forward declaration of Flash_Config. More...
 
typedef struct Flash_Params_s Flash_Params
 Forward declaration of Flash_Params. More...
 
Flash driver implementation callbacks
typedef int32_t(* Flash_OpenFxn) (Flash_Config *config, Flash_Params *params)
 Driver implementation to open a specific flash driver. More...
 
typedef void(* Flash_CloseFxn) (Flash_Config *config)
 Driver implementation to close a specific flash driver. More...
 
typedef int32_t(* Flash_ReadFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to read from flash using a specific flash driver. More...
 
typedef int32_t(* Flash_WriteFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to write to flash using specific flash driver. More...
 
typedef int32_t(* Flash_EraseFxn) (Flash_Config *config, uint32_t blockNum)
 Driver implementation to erase a block using a specific flash driver. More...
 

Functions

void Flash_Params_init (Flash_Params *params)
 Set default parameters in the Flash_Params structure. More...
 
Flash_Handle Flash_open (uint32_t instanceId, Flash_Params *params)
 Open flash driver. More...
 
void Flash_close (Flash_Handle handle)
 Close flash driver. More...
 
Flash_Handle Flash_getHandle (uint32_t instanceId)
 Get handle to flash driver. More...
 
int32_t Flash_read (Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Read data from flash. More...
 
int32_t Flash_write (Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Write to flash. More...
 
int32_t Flash_blkPageToOffset (Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
 Utility API to convert (Block Num, Page Num) to offset in bytes. More...
 
int32_t Flash_offsetToBlkPage (Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
 Utility API to convert offset in bytes to (Block Num, Page Num) More...
 
int32_t Flash_eraseBlk (Flash_Handle handle, uint32_t blockNum)
 Erase a block from flash. More...
 
uint32_t Flash_getPhyTuningOffset (Flash_Handle handle)
 Return flash offset to write PHY tuning data. More...
 
Flash_AttrsFlash_getAttrs (uint32_t instanceId)
 Return flash attributes. More...