PROFINET Device  v1.04.01
PN_API_SNMP_SPermanentData Struct Reference

#include <PN_API_SNMP.h>

Data Fields

uint16_t sysContactLength
 
uint8_t aSysContact [PN_API_SNMP_MAX_SNMP_SYSTEM_VALUE_BUFFER]
 
uint16_t sysNameLength
 
uint8_t aSysName [PN_API_SNMP_MAX_SNMP_SYSTEM_VALUE_BUFFER]
 
uint16_t sysLocationLength
 
uint8_t aSysLocation [PN_API_SNMP_MAX_SNMP_SYSTEM_VALUE_BUFFER]
 
uint16_t lldpMessageTxInterval
 
uint8_t lldpMessageTxHoldMultiplier
 
uint8_t lldpReinitDelay
 
uint16_t lldpTxDelay
 
uint16_t lldpNotificationInterval
 
PN_API_SNMP_SPort_t port1
 
PN_API_SNMP_SPort_t port2
 
uint8_t lldpConfigManAddrPortsTxEnable