IO-Link Master  1.04.06
SMI General

Overview

SMI General.

Typedefs

typedef void(* IOLM_SMI_CBGenericCnf) (IOLM_SMI_SHeader *psuHeader_p, INT8U *pu8ArgBlock_p)
 SMI Generic request confirmation callback. More...
 
typedef void(* IOLM_SMI_CBLoadMasterIdentification) (INT16U *u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
 Load Master configuration callback. More...
 
typedef void(* IOLM_SMI_CBLoadNVCfg) (INT8U u8Instance_p, INT8U *pu8Data_p, INT32U *pu32Length_p)
 Load configuration callback. More...
 
typedef void(* IOLM_SMI_CBSaveNVCfg) (INT8U u8Instance_p, INT8U *pu8Data_p, INT32U u32Length_p)
 Save configuration callback. More...
 
typedef void(* IOLM_SMI_CBSMIExt) (INT8U u8Instance_p, INT8U *pu8Data_p, INT16U u16Length_p)
 SMI extension function callback. More...
 

Functions

IOL_FUNC_DECL void IOLM_SMI_vGenericReq (IOLM_SMI_SHeader *psuHeader_p, INT8U *pu8ArgBlock_p)
 SMI generic request. More...
 
IOL_FUNC_DECL void IOLM_SMI_vSaveNvFinished (void)
 Save configuration finished. More...
 
void IOLM_SMI_vExtRsp (IOL_EErrorType eError_p, INT8U *pu8Data_p, INT16U u16Length_p)
 SMI extension response. More...
 
IOL_FUNC_DECL void IOLM_SMI_vRun (void)
 SMI Mainloop. More...
 
IOL_FUNC_DECL void IOLM_SMI_vInit (IOLM_SMI_SCallbacks *psuCallbacks_p)
 Initialize SMI interface. More...
 

Typedef Documentation

◆ IOLM_SMI_CBGenericCnf

IOLM_SMI_CBGenericCnf

SMI Generic request confirmation callback.

This callback function is called by the stack for a generic access of all services of the SMI. Confirmation to the IOLM_SMI_vGenericReq request.

Parameters
[in]psuHeader_pHeader.
[in]pu8ArgBlock_pGeneric ArgBlock.
Example
void IOLM_SMI_vGenericCnf(IOLM_SMI_SHeader *psuHeader_p, INT8U *pu8ArgBlock_p)
{
IOLM_SMI_SGeneralArgBlock *psuGenericArgBlock;
INT8U u16ArgBlockLength = psuHeader_p->u16ArgBlockLength;
psuGenericArgBlock = malloc(u16ArgBlockLength);
...
// Get header parameters
psuHeader_p->u8ClientId;
...
// Get ArgBlock data
memcpy(psuGenericArgBlock, pu8ArgBlock_p, u16ArgBlockLength);
// ToDo: Insert application specific code here
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

◆ IOLM_SMI_CBLoadMasterIdentification

IOLM_SMI_CBLoadMasterIdentification

Load Master configuration callback.

This callback service is called by the stack and requests the Master configuration from the application. Since this is hardware specific, it has to be implemented in the application code.

Parameters
[in]u16ArgBlockLength_pLength of the ArgBlock.
[in]pu8ArgBlock_pData pointer which points to the Master identification (IOLM_SMI_SMasterident).
Example
void IOLM_SMI_vLoadMasterIdentification(INT16U *u16ArgBlockLength_p, INT8U *pu8ArgBlock_p)
{
IOLM_SMI_SMasterident *psuMasterIdent = (IOLM_SMI_SMasterident *)pu8ArgBlock_p;
psuMasterIdent->u16ArgBlockID = IOLM_SMI_ENDIAN_16(IOLM_SMI_eArgBlockID_MasterIdent);
...
// ToDo: Set up psuMasterIdent parameters
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

◆ IOLM_SMI_CBLoadNVCfg

IOLM_SMI_CBLoadNVCfg

Load configuration callback.

This callback service is called by the stack and requests the saved configuration struct from non volatile memory. Since this is hardware specific, it has to be implemented in the application code.

Parameters
[in]u8Instance_p0-x for DataStorage Port and 0xFF for SMI configuration.
[in]pu8Data_pPointer to the configuration struct to be loaded (IOLM_SMI_SNVConfiguration).
[in]pu32Length_pPointer to the length of the configuration struct.
Example
void LOLM_SMI_vLoadNVCfg(INT8U u8Instance_p, INT8U *pu8Data_p, INT32U *pu32Length_p)
{
// Create local configuration struct in your application
IOLM_SMI_SNVConfiguration sNVConfiguration;
// Load configuration from non-volatile memory into struct
// ToDo: Insert hardware specific code here
// Copy configuration to pu8Data_p for the stack
memcpy(pu8Data_p, &sNVConfiguration, *pu32Length_p);
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

◆ IOLM_SMI_CBSaveNVCfg

IOLM_SMI_CBSaveNVCfg

Save configuration callback.

This callback service is called by the stack and is used to save the configuration struct to non volatile memory. If this function is finished writing the data it must call IOLM_SMI_vSaveNvFinished to notify the stack. Since this is hardware specific, it has to be implemented in the application code.

Parameters
[in]u8Instance_p0-x for Data Storage port and 0xFF for SMI configuration.
[in]pu8Data_pPointer to the configuration struct to be saved (IOLM_SMI_SNVConfiguration).
[in]u32Length_pLength of the configuration struct.
Example
void LOLM_SMI_vSaveNVCfg(INT8U u8Instance_p, INT8U *pu8Data_p, INT32U u32Length_p)
{
// Create local configuration struct in your application
IOLM_SMI_SNVConfiguration *psuNVConfiguration = (IOLM_SMI_SNVConfiguration *)pu8Data_p;
// Save configuration to non-volatile memory
// ToDo: Insert hardware specific code here
// Tell the stack that saving the configuration is finished
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

◆ IOLM_SMI_CBSMIExt

IOLM_SMI_CBSMIExt

SMI extension function callback.

Callback for extension functions which are proprietary and not included in the IOL/IOLW specification. Can be used for additional application specific services, firmware updates, etc. Since this is hardware specific, it has to be implemented in the application code.

Parameters
[in]u8Instance_pInstance (defined by caller).
[in]pu8Data_pPointer to the response data.
[in]u16Length_pLength of the response data
Example
void IOLM_SMI_vExtensionService(INT8U u8Instance_p, INT8U *pu8Data_p, INT16U u16Length_p)
{
IOL_EErrorType eErrorResponse;
INT8U *pu8DataResponse;
// ToDo: Insert application specific code here
// Response to stack
IOLM_SMI_vExtRsp(eErrorResponse, pu8DataResponse, 0);
}
See also
IOLM_SMI_SCallbacks, IOLM_SMI_vInit, IOLM_SMI_EArgBlockID

Function Documentation

◆ IOLM_SMI_vExtRsp()

void IOLM_SMI_vExtRsp ( IOL_EErrorType  eError_p,
INT8U pu8Data_p,
INT16U  u16Length_p 
)

SMI extension response.

Responses of extension functions which are proprietary and not included in the IOL/IOLW specification.

Parameters
[in]eError_pError message as IOL_EErrorType.
[in]pu8Data_pPointer to the response data.
[in]u16Length_pLength of the response data
Example
void IOLM_SMI_vExtensionService(INT8U u8Instance_p, INT8U *pu8Data_p, INT16U u16Length_p)
{
IOL_EErrorType eErrorResponse;
INT8U *pu8DataResponse;
// ToDo: Insert application specific code here
// Response to stack
IOLM_SMI_vExtRsp(eErrorResponse, pu8DataResponse, 0);
}
See also
IOLM_SMI_CBSMIExt

◆ IOLM_SMI_vGenericReq()

IOL_FUNC_DECL void IOLM_SMI_vGenericReq ( IOLM_SMI_SHeader psuHeader_p,
INT8U pu8ArgBlock_p 
)

SMI generic request.

The function is used for a generic access of all services of the SMI. The answer to this request is the callback function IOLM_SMI_CBGenericCnf.

Parameters
[in]psuHeader_pHeader.
[in]pu8ArgBlock_pGeneric ArgBlock.
Example
// Allocate header memory
INT8U au8HeaderMem[sizeof(IOLM_SMI_SHeader)];
IOLM_SMI_SHeader *psuHeader = (IOLM_SMI_SHeader *)au8HeaderMem;
// Allocate ArgBlock memory (pu8Data contains the data of length u16DataLength)
INT16U u16ArgBlockLength = sizeof(IOLM_SMI_SGeneralArgBlock) + u16DataLength;
INT8U au8ArgBlockMem[u16ArgBlockLength];
IOLM_SMI_SGeneralArgBlock *psuArgblock = (IOLM_SMI_SGeneralArgBlock *)au8ArgBlockMem;
// Fill header
psuHeader->u16ArgBlockLength = u16ArgBlockLength;
psuHeader->u8Service = ...
...
// Fill request
psuArgblock->u16ArgBlockID = IOLM_SMI_ENDIAN_16(IOLM_SMI_SGeneralArgBlock); // ArgBlock ID (little endian)
...
// Copy user data into ArgBlock request
memcpy(psuArgblock + sizeof(IOLM_SMI_SGeneralArgBlock), pu8Data, u16ArgBlockLength);
// ToDo: Insert application specific code here
// Send request
IOLM_SMI_vGenericReq(psuHeader, (INT8U *)psuArgblock);
// wait for IOLM_SMI_CBGenericCnf

◆ IOLM_SMI_vInit()

IOL_FUNC_DECL void IOLM_SMI_vInit ( IOLM_SMI_SCallbacks psuCallbacks_p)

Initialize SMI interface.

Initializes the SMI Interface, sets initial values, loads saved configuration (if present), etc. Must be called once before SMI Mainloop (IOLM_SMI_vRun).

Parameters
[in]psuCallbacks_pSet of callback functions.
Example
// ToDo: Setup the desired callbacks
IOLM_SMI_SCallbacks suSMICallbacks_g =
{
.cbGenericCnf = IOLM_SMI_cbGenericCnf,
.cbPortConfigurationCnf = IOLM_SMI_cbPortConfigurationCn,
.cbReadbackPortConfigurationCnf = IOLM_SMI_cbReadbackPortConfigurationCnf,
.cbPortStatusCnf ...
...
};
// Initialize stack and SMI (suSMICallbacks_g must be global)
IOLM_SMI_vInit(&suSMICallbacks_g);
// Application Mainloop
while (1)
{
IOLM_SMI_vRun(); // SMI Mainloop (at least once per ms)
User_Application(); // ToDo: Insert application specific code here
}
See also
IOLM_SMI_SCallbacks

◆ IOLM_SMI_vRun()

IOL_FUNC_DECL void IOLM_SMI_vRun ( void  )

SMI Mainloop.

Runs periodically to execute the next jobs in the queue, etc. Must be called at least once every millisecond to guarantee a stable stack environment.

Example
// ToDo: Setup the desired callbacks
IOLM_SMI_SCallbacks suSMICallbacks_g =
{
.cbGenericCnf = IOLM_SMI_vGenericCnf,
.cbMemFree = IOLM_SMI_vMemFree,
.cbMemAlloc = LOLM_SMI_pu8ArgBlockAlloc,
.cbLoadNvCfg = ...
...
};
// Initialize stack and SMI (suSMICallbacks_g must be global)
IOLM_SMI_vInit(&suSMICallbacks_g);
// Application Mainloop
while (1)
{
IOLM_SMI_vRun(); // SMI Mainloop (at least once per ms)
User_Application(); // ToDo: Insert application specific code here
}

◆ IOLM_SMI_vSaveNvFinished()

IOL_FUNC_DECL void IOLM_SMI_vSaveNvFinished ( void  )

Save configuration finished.

This service needs to be called by the application code, to inform the stack, that the configuration is successfully written to the non volatile memory function in the application code (which can take a few hundred milliseconds).

void LOLM_SMI_vSaveNVCfg(INT8U u8Instance_p, INT8U *pu8Data_p, INT32U u32Length_p)
{
// Create local configuration struct in your application
IOLM_SMI_SNVConfiguration *psuNVConfiguration = (IOLM_SMI_SNVConfiguration *)pu8Data_p;
// Save configuration to non-volatile memory
// ToDo: Insert hardware specific code here
// Tell the stack that saving the configuration is finished
}
See also
IOLM_SMI_CBSaveNVCfg
IOLM_SMI_SCallbacks::cbGenericCnf
IOLM_SMI_CBGenericCnf cbGenericCnf
Callback for IOLM_SMI_vGenericReq.
Definition: IOLM_SMI.h:2300
IOLM_SMI_SCallbacks
SMI Callbacks. Must be initialized via IOLM_SMI_vInit.
Definition: IOLM_SMI.h:2298
INT32U
uint32_t INT32U
32 bit unsigned integer
Definition: IOL_Port_Types.h:72
IOLM_SMI_vRun
void IOLM_SMI_vRun(void)
SMI Mainloop.
Definition: IOLM_SMI.c:2660
IOLM_SMI_SVoidArgBlock::u16ArgBlockID
INT16U u16ArgBlockID
Big endian.
Definition: IOLM_SMI_Types.h:353
IOL_EErrorType
IOL_EErrorType
This enumeration indicates the permissible ISDU ErrorTypes resulting from the Device application.
Definition: IOL_Types.h:541
IOLM_SMI_vSaveNvFinished
void IOLM_SMI_vSaveNvFinished(void)
Save configuration finished.
Definition: IOLM_SMI.c:418
IOLM_SMI_SVoidArgBlock
This structure is used as general and void ArgBlock.
Definition: IOLM_SMI_Types.h:352
IOLM_SMI_SNVConfiguration
Definition: IOLM_SMI.h:302
IOLM_SMI_vGenericReq
void IOLM_SMI_vGenericReq(IOLM_SMI_SHeader *psuHeader_p, INT8U *pu8ArgBlock_p)
SMI generic request.
Definition: IOLM_SMI.c:2868
IOLM_SMI_vInit
void IOLM_SMI_vInit(IOLM_SMI_SCallbacks *psuCallbacks_p)
Initialize SMI interface.
Definition: IOLM_SMI.c:294
IOLM_SMI_SMasterident::u16ArgBlockID
INT16U u16ArgBlockID
Big endian.
Definition: IOLM_SMI_Types.h:378
IOLM_SMI_vExtRsp
void IOLM_SMI_vExtRsp(IOL_EErrorType eError_p, INT8U *pu8Data_p, INT16U u16Length_p)
SMI extension response.
Definition: IOLM_SMI.c:1714
INT16U
uint16_t INT16U
16 bit unsigned integer
Definition: IOL_Port_Types.h:70
IOLM_SMI_SHeader
This structure is used for the SMI_Header.
Definition: IOLM_SMI_Types.h:808
IOLM_SMI_SHeader::u16ArgBlockLength
INT16U u16ArgBlockLength
Little endian.
Definition: IOLM_SMI_Types.h:815
IOLM_SMI_SHeader::u8ClientId
INT8U u8ClientId
Client id. IOLM_SMI_CLIENTID_INTERN and IOLM_SMI_CLIENTID_BROADCAST are reserved.
Definition: IOLM_SMI_Types.h:814
IOLM_SMI_SMasterident
This structure is used to get Master identification.
Definition: IOLM_SMI_Types.h:377
INT8U
uint8_t INT8U
8 bit unsigned integer
Definition: IOL_Port_Types.h:68