EtherNet/IP™ Adapter  1.03.04
User Reference Manual

◆ EI_API_CIP_ESc

Available CIP service codes.

Specifies which services are available on the CIP class or instance.

Enumerator
EI_API_CIP_eSC_GETATTRIBUTESALL 

Returns the contents of the instance or class attributes defined in the object definition.

EI_API_CIP_eSC_RESET 

Perform a reset.

EI_API_CIP_eSC_GETATTRSINGLE 

Get_Attribute_Single is used to return the content of the specified attribute.

EI_API_CIP_eSC_SETATTRSINGLE 

Set_Attribute_Single must be set if the attribute value should be modified.