EtherNet/IP™ Adapter  1.03.04
User Reference Manual

◆ EI_API_ADP_getEnipAcdState()

uint32_t EI_API_ADP_getEnipAcdState ( T pAdp_p,
uint8_t *  pEnipAcdState_p 
)

Get the current adapter Ethernet IP address conflict detection status (Instance Attribute ID: 11).

This function returns the adapter Ethernet IP address conflict detection status in parameter pEnipAcdState_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pEnipAcdState_puint8_t pointer to adapter address conflict detection status for the adapter specified by parameter pAdp_p.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t enipAcdState;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getEnipAcdState(pEI_API_ADP, &enipAcdState);
See also
EI_API_ADP_setEnipAcdState EI_API_ADP_EError_t
EI_API_ADP_getEnipAcdState
ETHIP_API uint32_t EI_API_ADP_getEnipAcdState(T *pAdp_p, uint8_t *pEnipAcdState_p)
Get the current adapter Ethernet IP address conflict detection status (Instance Attribute ID: 11).
Definition: EI_API_ADP_main.c:2974
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:219