EtherNet/IP™ Adapter  1.03.04
User Reference Manual

◆ EI_API_ADP_getIpTTL()

uint32_t EI_API_ADP_getIpTTL ( T pAdp_p,
uint8_t *  pIpTTL_p 
)

Get the current TTL value (Instance Attribute ID: 8).

Function that returns the Time to Live (TTL) value.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pIpTTL_puint32_t pointer to TTL value of the adapter specified by parameter pAdp_p.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t adpIpTTL;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getIpTTL(pEI_API_ADP, &adpIpTTL);
See also
EI_API_ADP_setIpTTL EI_API_ADP_EError_t
EI_API_ADP_getIpTTL
ETHIP_API uint32_t EI_API_ADP_getIpTTL(T *pAdp_p, uint8_t *pIpTTL_p)
Get the current TTL value (Instance Attribute ID: 8).
Definition: EI_API_ADP_main.c:2588
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:219