EtherCAT Slave  1.04.05

◆ EC_API_SLV_setStandardMailbox()

uint32_t EC_API_SLV_setStandardMailbox ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint16_t  rxOffset_p,
uint16_t  rxSize_p,
uint16_t  txOffset_p,
uint16_t  txSize_p 
)

Set Standard Mailbox Configuration.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]rxOffset_pStart offset of bootstrap Receive Mailbox.
[in]rxSize_pSize of bootstrap Receive Mailbox.
[in]txOffset_pStart offset of bootstrap Send Mailbox.
[in]txSize_pSize of bootstrap Send Mailbox.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_setStandardMailbox(S_ecSlvApiHdl, 0x1000, 256, 0x1100, 256);
See also
EC_API_SLV_setBootStrapMailbox
Examples
ecSlvCiA402.c.
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134
EC_API_SLV_setStandardMailbox
uint32_t EC_API_SLV_setStandardMailbox(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t rxOffset_p, uint16_t rxSize_p, uint16_t txOffset_p, uint16_t txSize_p)
Set Standard Mailbox Configuration.
Definition: ecSlvApi_ParamStub.c:606