EtherCAT Slave  1.04.05

◆ EC_API_SLV_init()

uint32_t EC_API_SLV_init ( EC_API_SLV_SHandle_t pEcSlaveApi_p)

This is the function to initialize the EtherCAT Slave API.

If an instance was created it can be initialized with this function. If there is no error the instance is ok to run.

Parameters
[in]pEcSlaveApi_pAPI instance handle.
Returns
EC_API_EError_t Returns the API error code..
Example
#include <ecSlvApi.h>
// required variables
EC_API_EError_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_init(S_ecSlvApiHdl);
See also
EC_API_SLV_run
Examples
ecSlvCiA402.c, and ecSlvESI.c.
EC_API_EError_t
enum EC_API_EError EC_API_EError_t
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134
EC_API_SLV_init
uint32_t EC_API_SLV_init(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
This is the function to initialize the EtherCAT Slave API.
Definition: ecSlvApiStub.c:679