Data Fields | |
SA2UL_SecCtx | secCtx |
uint8_t | secCtxId |
SA2UL_Handle | handle |
SA2UL_ContextParams | ctxPrms |
uint32_t | totalLengthInByes |
uint8_t | computedHash [SA2UL_MAX_HASH_SIZE_BYTES] |
uint32_t | computationStatus |
uint32_t | txBytesCnt |
uint32_t | rxBytesCnt |
uint32_t | sa2ulErrCnt |
SA2UL_SecCtx SA2UL_ContextObject::secCtx |
uint8_t SA2UL_ContextObject::secCtxId |
SA2UL_Handle SA2UL_ContextObject::handle |
SA2UL_ContextParams SA2UL_ContextObject::ctxPrms |
SA2UL secure parameter as provided by user
uint32_t SA2UL_ContextObject::totalLengthInByes |
uint8_t SA2UL_ContextObject::computedHash[SA2UL_MAX_HASH_SIZE_BYTES] |
uint32_t SA2UL_ContextObject::computationStatus |
uint32_t SA2UL_ContextObject::txBytesCnt |
uint32_t SA2UL_ContextObject::rxBytesCnt |
uint32_t SA2UL_ContextObject::sa2ulErrCnt |