Parameters passed during Crypto_shaOpen()
Data Fields | |
uint32_t | authMode |
uint32_t | type |
uint32_t Crypto_ShaParams::authMode |
Authentication mode. Refer Crypto_ShaAuthMode
uint32_t Crypto_ShaParams::type |
Type to which to assign the context. Refer Crypto_Type