|
| enum | nodeState { NODE_IDLE = 0,
NODE_FAULT = 1,
NODE_NORMAL = 2
} |
| | node state machine states More...
|
| |
| enum | ringState { RING_NORMAL = 1,
RING_FAULT = 2
} |
| | ring state values More...
|
| |
| enum | nwTopology { LINEAR_TOP = 0,
RING_TOP = 1
} |
| | network topology : possible values for Attribute ID 1 More...
|
| |
| enum | nwStatus {
NORMAL_STAT = 0,
RING_FAULT_STAT = 1,
UNEXPECTED_LOOP = 2,
PARTIAL_FAULT = 3,
RAPID_FAULT = 4
} |
| | network status : possible values for Attribute ID 2 More...
|
| |
| enum | supervisorStatus {
BACKUP_NODE = 0,
ACTIVE_RING_SUPERVISOR = 1,
RING_NODE = 2,
NON_DLR = 3,
FEATURE_UNSUPPORTED = 4
} |
| | device role: possible values for Attribute ID 3 More...
|
| |
|
| void | EIP_DLR_init (EIP_DLRHandle dlrHandle) |
| | API to initialize the DLR driver. More...
|
| |
| void | EIP_DLR_start (EIP_DLRHandle dlrHandle) |
| | API to start the DLR driver Calling this enables DLR on the device. More...
|
| |
| void | EIP_DLR_stop (EIP_DLRHandle dlrHandle) |
| | API to stop the DLR driver Halt DLR. Calling this disables DLR on the device. More...
|
| |
| void | EIP_DLR_port0ISR (uintptr_t arg) |
| | Fast ISR for Port 0, bypasses the buffer copy and NDK. More...
|
| |
| void | EIP_DLR_port1ISR (uintptr_t arg) |
| | Fast ISR for Port 1, bypasses the buffer copy and NDK. More...
|
| |
| void | EIP_DLR_beaconTimeoutISR_P0 (uintptr_t arg) |
| | ISR for beacon timeout for Port 0. More...
|
| |
| void | EIP_DLR_beaconTimeoutISR_P1 (uintptr_t arg) |
| | ISR for beacon timeout for Port 1. More...
|
| |
| void | EIP_DLR_port0ProcessLinkBrk (uint8_t linkStatus, void *arg2) |
| | Process DLR state machine in the event of a link break on Port0. More...
|
| |
| void | EIP_DLR_port1ProcessLinkBrk (uint8_t linkStatus, void *arg2) |
| | Process DLR state machine in the event of a link break on Port1. More...
|
| |
| void | EIP_DLR_neighborTimeoutISR0 (ClockP_Object *obj, void *arg) |
| | ISR for Neighbor timeout timer for port 0. More...
|
| |
| void | EIP_DLR_neighborTimeoutISR1 (ClockP_Object *obj, void *arg) |
| | ISR for Neighbor timeout timer for port 1. More...
|
| |
| void | EIP_DLR_addVlanID (uint8_t *src, uint16_t vlanID) |
| |
| void | EIP_DLR_genNCReqFrame (EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort) |
| |
| void | EIP_DLR_genNCResFrame (uint8_t *src, uint8_t sourcePort, uint8_t reqSrcPort, uint32_t sequenceId) |
| |
| void | EIP_DLR_genNeighborLinkStatFrame (EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort, uint8_t linkOrNeighbor, uint8_t linkStatus) |
| |
| void | EIP_DLR_initDLRFrameHeader (uint8_t *src, uint8_t *header) |
| |
| void | EIP_DLR_addSignOnNumNodes (uint8_t *src, uint16_t numNodes) |
| |
| void | EIP_DLR_processDLRFrame (EIP_DLRHandle dlrHandle, uint8_t *pktBuffer, uint8_t portNum, uint16_t size) |
| | Processes a sign on and Neighbor check request frame. More...
|
| |
| void | EIP_DLR_dRAMInit (EIP_DLRHandle dlrHandle) |
| |
| void | EIP_DLR_resetStateMachine (EIP_DLRHandle dlrHandle) |
| | Initialize the state machine when it goes back to idle state. More...
|
| |
| void | EIP_DLR_setDefaultValue (EIP_DLRHandle dlrHandle) |
| |
| void | EIP_DLR_switchToFault (EIP_DLRHandle dlrHandle) |
| |
| void | EIP_DLR_switchToNormal (EIP_DLRHandle dlrHandle) |
| |
| int32_t | EIP_DLR_isrInit (EIP_DLRHandle dlrHandle) |
| |
| void | EIP_DLR_periodicProcessing (ClockP_Object *obj, void *userArg) |
| |
| void | EIP_DLR_addToExceptionList (EIP_DLRHandle dlrHandle, uint8_t *macId) |
| |
| void | EIP_DLR_clearExceptionList (EIP_DLRHandle dlrHandle) |
| |
| uint8_t | EIP_DLR_checkSupervisorException (uint8_t *macId, EIP_DLRHandle dlrHandle) |
| |
| void | EIP_DLR_addModuleIPAddress (EIP_DLRHandle dlrHandle, uint32_t newIP) |
| |
| void | EIP_DLR_setDivider_WD_IEP (EIP_DLRHandle dlrHandle) |
| | Sets the clock divider to 1us for IEP watch dog timers. More...
|
| |
| void | EIP_DLR_enable_WD_IEP (EIP_DLRHandle dlrHandle, uint8_t id) |
| | Enable the IEP Watch dog timers. More...
|
| |
| void | EIP_DLR_disable_WD_IEP (EIP_DLRHandle dlrHandle, uint8_t id) |
| | Disable the IEP Watch dog timers. More...
|
| |
| void | EIP_DLR_setTimeout_WD_IEP (EIP_DLRHandle dlrHandle, uint16_t periodInMicroSec, uint8_t id) |
| | Set the timeout value in watchdog. More...
|
| |
| void | EIP_DLR_set_pdi_wd_trigger_mode (EIP_DLRHandle dlrHandle, uint32_t mode) |
| | Set the PDI WD trigger mode. More...
|
| |