General Interface attribute parameter collection. More...
#include <EI_API_def.h>
Data Fields | |
uint8_t | ETHIntfActive: 1 |
1 Is the interface activated? More... | |
uint8_t | ETHIntfAutoNeg: 1 |
2 Is auto neg. on More... | |
uint8_t | ETHIntfFDuplex: 1 |
3 Is full duplex More... | |
uint8_t | ETHIntf100MB: 1 |
4 Is 100 mbit More... | |
uint8_t | rsvd: 4 |
5:8 Reserved More... | |
General Interface attribute parameter collection.