uint32_t EI_API_CIP_NODE_delete | ( | T * | pCipNode_p | ) |
Delete the CIP node specified by parameter pCipNode_p
.
If a CIP node was created it can be deleted with this function. The memory which was allocated by the CIP node will be freed.
[in] | pCipNode_p | Pointer to the CIP node. |
EI_API_CIP_eERR_OK | Success. |
EI_API_CIP_eERR_NODE_INVALID | CIP node is invalid, possibly EI_API_CIP_NODE_new() was not called. |