#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId = 0x0064;
uint16_t instanceId = 0x01;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:195
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition: EI_API_CIP_main.c:354
@ EI_API_CIP_eAR_GET
Attribute is gettable.
Definition: EI_API_def.h:130
@ EI_API_CIP_eEDT_UINT
Definition: EI_API_CIP.h:128
@ EI_API_CIP_eCDT_NO
Definition: EI_API_CIP.h:163
ETHIP_API uint32_t EI_API_CIP_createInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p)
Creates a CIP instance.
Definition: EI_API_CIP_main.c:898
ETHIP_API uint32_t EI_API_CIP_addInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Add an attribute to an instance.
Definition: EI_API_CIP_main.c:1447
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_main.c:69
EI_API_CIP_EEdt_t edt
Definition: EI_API_CIP.h:194
EI_API_CIP_EAr_t accessRule
Definition: EI_API_CIP.h:196
uint16_t id
Definition: EI_API_CIP.h:193
EI_API_CIP_ECdt_t cdt
Definition: EI_API_CIP.h:195
uint16_t cdtSize
Definition: EI_API_CIP.h:198
uint16_t edtSize
Definition: EI_API_CIP.h:197
General attribute parameter collection.
Definition: EI_API_CIP.h:192